The goal is net-zero emissions: the first phase has already reduced the university's carbon footprint by 10%.
The University of East London has set itself the ambitious goal of achieving net-zero emissions by 2030. Recognized as one of the best universities in the British capital, the institution has developed a comprehensive roadmap to achieve this target.
As a first step, the university assessed how its various spaces were being used and identified opportunities for energy savings across its buildings. By installing approximately 11,000 LED lights and upgrading the building management system at 35 points, the institution was able to optimize its energy consumption and achieve a 10% reduction in CO2 emissions across its Docklands and Stratford campuses, which serve 25,000 students.
The second phase focuses on the transition to clean energy. A solar power system with a total capacity of 2 megawatts has been installed across the campuses, capable of generating up to 1.2 GWh (gigawatt-hours) of carbon-free electricity annually. According to the university's calculations, 90% of this electricity will be consumed on-site, while the remainder can be fed back into the public electricity grid, similar to the way microgrids operate. Heat pumps and 27 new electric vehicle charging points have also been installed.
The university, which educates 40,000 students, is also integrating sustainability into everyday campus life. By incorporating sustainability into its curriculum, the institution aims to inspire students and equip them with valuable knowledge and skills to succeed in the green economy and make environmentally responsible use of intelligent, IoT-based digital technologies. A community program for green energy startups has also been launched.
These initiatives have helped the university's carbon reduction program, launched three years ago and implemented using Siemens technology, earn the UK's Net Zero Leader Award.