Comunicado de prensa

H2 Core Systems builds scalable hydrogen energy solutions with Siemens Xcelerator

18 de mayo de 2026
Plano, Texas, USA

H2 Core Systems is using the Siemens Xcelerator platform of software and automation portfolio to design and manufacture compact, highly efficient hydrogen energy systems that generate and store clean energy (Image credit: H2 Core Systems)
  • Siemens’ software and automation portfolio enables modular hydrogen energy system manufacturer to accelerate design, eliminate production errors and respond to customer demands for custom solutions
  • Digital workflow with Designcenter X and Teamcenter Share accelerates design and customization by 20 percent and helps to halve production time

Siemens has announced that H2 Core Systems, a startup focused on modular hydrogen-based energy systems, is using the Siemens Xcelerator platform of software and automation portfolio to design and manufacture compact, highly efficient hydrogen energy systems that generate and store clean energy where it is needed.

H2 Core Systems is leveraging Siemens’ Designcenter™ X Solid Edge® software as the backbone of its fully digital product development process, enabling it to design and visualize its products in 3D before physical production. The digital workflow has enabled it to reduce production time by 50 percent, speed up design and customization cycles by 20 percent and achieve an overall growth rate of 70 percent. Designcenter X Solid Edge, in combination with the cloud-based collaboration capabilities of Siemens’ Teamcenter® Share app, allows the team to create marketing assets, technical documentation and aids communication of complex design concepts clearly to customers and stakeholders.

siemens-h2-core-systems-newsroom-02-1280x720

H2 Core Systems is using the Siemens Xcelerator platform of software and automation portfolio to design and manufacture compact, highly efficient hydrogen energy systems that generate and store clean energy (Image credit: H2 Core Systems)

H2 Core Systems also takes advantage of Siemens’ automation hardware and software, including S7 1200 compact programmable logic controllers (PLCs) and TIA Portal to develop and implement the automation its complex products required.

Founded in 2019 and based in Heide, Germany, H2 Core Systems develops, manufactures and maintains modularly configurable production, storage and energy systems that combine electrolysis with storage, compression, fuel cells and everything around a hydrogen-based eco-system. Designed to be flexible, expandable and scalable, alongside on-grid use its products are perfect for combination with photovoltaic or wind power systems in a decentralized, self-sufficient and green energy supply that can be used worldwide.

“In our role as an accelerator of the energy transition, we need to respond to individual requirements promptly and with modular, scalable energy systems,” said Ulf Jörgensen, chief executive officer, H2 Core Systems. “This acceleration is based on fully digitalized, dynamic and efficient collaboration between sales, engineering, production and documentation. Siemens Xcelerator enables this collaboration and significantly reduces our time-to-market.”

siemens-h2-core-systems-newsroom-03-1280x720

H2 Core Systems is using the Siemens Xcelerator platform of software and automation portfolio to design and manufacture compact, highly efficient hydrogen energy systems that generate and store clean energy (Image credit: H2 Core Systems)

"Siemens Xcelerator, including Designcenter and Teamcenter, is built to help companies like H2 Core Systems design and collaborate more efficiently; by allowing them to visualize the complete product in 3D and collaborate seamlessly with stakeholders from anywhere, on any device, they can make informed design changes before production starts, saving time and money. This speeds the development of new solutions, allows greater innovation and enables customization based on customer needs," said Joe Bohman, EVP PLM Products, Siemens Digital Industries Software. "Siemens' technologies help them reduce complex steps and deliver sustainable energy systems quickly to communities that need them."

A recent project saw H2 Core Systems design and build a fully autonomous energy system for a school in Niger. The result is an independent, emission-free power supply where solar energy is used to split water into hydrogen and oxygen. The green hydrogen produced is stored and can later be converted back into electricity when needed, resulting in an independent, emission-free power supply – without diesel, without unstable grids, and without long fossil fuel supply chains.

siemens-h2-core-systems-newsroom-04-1280x720

Digital workflow with Designcenter X Solid Edge and Teamcenter Share accelerates design and customization by 20 percent and helps to halve production time (Image credit: H2 Core Systems)

“By combining modular hydrogen energy systems with Siemens’ advanced software and automation hardware, we can continue to deliver sustainable energy solutions worldwide, quickly adapting to customer needs and scaling our impact,” says Thorsten Claussen, head of mechanical engineering, H2 Core Systems. “We use Designcenter X Solid Edge to fully digitize our dynamic product and production planning. Thanks to the innovative solutions for distributed teams and high variability, we can significantly accelerate our development processes and production preparations and thus considerably reduce the time-to-market of our hydrogen-based energy systems.”

To learn more about H2 Core Systems and its adoption of the Siemens Xcelerator portfolio of software and automation hardware, watch the video on YouTube or visit https://resources.sw.siemens.com/en-US/case-study-h2-core-systems/

Siemens AG (Berlin y Munich) es una empresa tecnológica líder centrada en la industria, las infraestructuras, la movilidad y la salud. El objetivo de la empresa es crear tecnología para transformar el día a día de todos. Al combinar el mundo real y el digital, Siemens permite a sus clientes acelerar su transformación digital y sostenible, haciendo que las fábricas sean más eficientes, las ciudades más habitables y el transporte más sostenible. Siemens también posee una participación mayoritaria en la empresa cotizada Siemens Healthineers, un proveedor líder mundial de tecnología médica pionero en avances en el ámbito de la salud. Para todos. En todas partes. De forma sostenible.

En el ejercicio fiscal 2025, que finalizó el 30 de septiembre de 2025, el Grupo Siemens generó unos ingresos de 78 900 millones de euros y un beneficio neto de 10 400 millones de euros. A 30 de septiembre de 2025, la empresa empleaba a unas 318 000 personas en todo el mundo sobre la base de operaciones continuadas. Para más información, visite www.siemens.com.

Siemens Digital Industries (DI) empowers companies of all sizes within the process and discrete manufacturing industries to accelerate their digital and sustainability transformation across the entire value chain. Siemens’ cutting-edge automation and software portfolio revolutionizes the design, realization and optimization of products and production. And with Siemens Xcelerator – the open digital business platform – this process is made even easier, faster, and scalable. Together with our partners and ecosystem, Siemens Digital Industries enables customers to become a Digital Enterprise. Siemens Digital Industries has a workforce of around 70,000 people worldwide.

Siemens Digital Industries Software ayuda a organizaciones de todos los tamaños a transformarse digitalmente utilizando software, hardware y servicios de la plataforma empresarial Siemens Xcelerator. El software de Siemens y el gemelo digital completo permiten que las empresas optimicen sus procesos de diseño, ingeniería y fabricación para convertir las ideas de hoy en los productos sostenibles del futuro. Desde los chips hasta los sistemas completos, desde el producto hasta el proceso, en todos los sectores. Siemens Digital Industries Software – Accelerating transformation.

H2 Core Systems is a global manufacturer of hydrogen systems. H2 Core Systems sets the standard for the future and is the top choice for self-sufficient H2 production and energy independence through safe and cost-effective hydrogen system solutions. H2 Core implements scalable H2 system solutions for true autonomy and independence from resources and prices. Through the intelligent integration of generation, storage, and reconversion to electricity, H2 Core guarantees maximum supply security with full cost control. Made in Germany, plug-and-play ready, modularly scalable, and CO2-free when combined with renewable energy. H2 Core Systems is an all-in-one provider and supports customers across the entire value chain, from consulting and engineering through production to installation, service, and maintenance. www.h2coresystems.com

Persona de contacto para la prensa

Siemens Digital Industries Software PR Team
press.software.sisw@siemens.com