Pressiteade

Do we still need separate summer and winter tires?

24. september 2024
Hungary

Source of the images: Michelin Hungária

5+1 surprising facts you probably didn't know about tires

What tires do electric vehicles need? How can tires help reduce a vehicle's energy consumption? What do the markings on tire sidewalls mean, and what revolutionary changes are taking place in tire manufacturing? In the latest episode of the Voices of Industry podcast, Dr. Attila Nemes, Managing Director of Michelin Hungária, shares fascinating insights into tire technology and the operations of the company's Nyíregyháza factory.

Aerial view of flat-roofed industrial buildings with yellow accents, parking lots, and trees under an orange-yellow sunset.

1. How tire materials have changed over 150 years

Technological advances in the tire industry are also reflected in the materials used in manufacturing. Natural rubber and carbon black are increasingly being supplemented or replaced by bio-based and recyclable materials in modern tires, helping to extend their lifespan and reduce their environmental impact. Michelin aims to make its tires fully recyclable by 2050. “Today, 40% of our tires are made from recycled materials, and we are continuously working to increase this proportion,” explained Dr. Attila Nemes, Managing Director of Michelin Hungária, in the Voices of Industry podcast.

2. Rolling resistance: The hidden factor behind fuel consumption

While many motorists closely follow fluctuations in fuel prices, few realize that tire rolling resistance can account for as much as 20% of a car's fuel consumption. “One out of every five tanks of fuel is effectively 'consumed' by the tires. By reducing rolling resistance, we can make vehicles more efficient,” explained Dr. Attila Nemes.

Industrial apparatus supports three upside-down treaded tires; cylinder, reflective glass, and part of a person are visible.

What else can tires tell us?

In addition to the standard tire size, speed rating and DOT manufacturing date code, modern tires provide valuable information about their construction and the materials used. Markings on the sidewall also include weather-related classifications, helping drivers determine the conditions for which a tire is suitable. Tires may also carry regional homologation markings indicating the geographical markets in which they comply with regulatory requirements.

  • Size: The numbers and letters on a tire's sidewall indicate its width, aspect ratio and diameter. For example, “205/55 R16” means the tire is 205 mm wide, has an aspect ratio of 55%, features radial construction and fits a 16-inch wheel rim.
  • Speed rating: A letter indicates the maximum speed at which a tire can safely operate. For example, “H” corresponds to 210 km/h, “V” to 240 km/h and “Y” to 300 km/h.
  • DOT code: One of the most important markings is the manufacturing date, indicated by the DOT code. This helps determine when the tire was produced and assess whether it is still suitable for safe use. The first two digits of the four-digit date code indicate the production week, while the last two indicate the year of manufacture.
  • XL (Extra Load): A reinforced tire with a higher load-carrying capacity than a standard tire of the same size.
  • RF (Reinforced): A reinforced tire, similar to an XL-rated tire. The RF designation may reflect different terminology used by manufacturers. These tires are designed for increased load capacity and stability.
  • TWI (Tread Wear Indicator): Markings indicating the location of tread wear indicators, which help drivers monitor tire wear. The indicators are located in the tire's tread grooves.
  • TL (Tubeless): Indicates that the tire does not require an inner tube, as its airtight construction is integrated into the tire itself.
  • M+S (Mud + Snow): A marking commonly found on winter and all-season tires, indicating that the tire is designed for use in mud and snow.
  • All Season / All Weather: Indicates an all-season tire designed to perform in a variety of weather conditions, including rain, snow and dry conditions.

Michelin Nyiregyhaza 03

3. What tires should we choose for electric vehicles?

Many electric vehicle owners wonder which tires will ensure optimal performance. Electric cars differ from conventional gasoline and diesel vehicles in several ways, and these differences also influence tire selection. First, electric vehicles deliver particularly high torque, which can cause tires to wear more quickly and intensively. Second, their batteries make them heavier than conventional vehicles, requiring tires with a higher load-carrying capacity. Nevertheless, according to Michelin's expert, it is not necessary to choose tires specifically designed for electric vehicles. All Michelin tires are engineered to meet the performance requirements of electric cars, making them suitable for both electric and conventional vehicles.

4. From rubber balls to Porsche tires

Surprisingly, Michelin's Nyíregyháza factory did not originally manufacture tires at all. The facility initially produced red polka-dot rubber balls and various industrial rubber products before beginning tractor tire production in 1979. A major turning point came in 1996, when the factory joined the Michelin Group. In 2005, it transitioned to manufacturing passenger car tires. Today, the plant supplies premium automotive brands such as Porsche, Ferrari and Land Rover, producing approximately two million high-performance tires annually.

A person in a blue short-sleeved shirt, blue pants, and belt works on a tire mounted on machinery.

5. Separate summer and winter tires may no longer be necessary in Hungary

Every spring and autumn, seasonal tire changes present a familiar dilemma for motorists. It is no coincidence that all-season tires are becoming increasingly popular, offering a practical solution for year-round driving. For many years, however, experts emphasized the importance of seasonal tire changes and dedicated winter tires. Speaking on the Voices of Industry podcast, Michelin's Managing Director explained that Hungary's climate makes all-season tires a particularly suitable option. “These tires perform well in summer, while winter conditions in Hungary are generally not extreme enough to require the additional performance of dedicated winter tires,” added Dr. Attila Nemes.

5+1. Electricity replaces steam and gas in tire vulcanization

Sustainability has also become a major priority in the tire industry. In recent years, Michelin's Nyíregyháza factory has undergone significant changes aimed at improving energy efficiency and sustainability. One of the key stages of tire manufacturing is vulcanization, a process traditionally carried out using steam. The factory has now transformed this process by switching from gas-based heating to electricity. In cooperation with Siemens, the vulcanization presses were converted to operate directly using electrical energy. The factory is also increasingly adopting robotic processes, which not only improve production efficiency but also reduce the physical workload of employees. The tire-handling robots are also operated using Siemens control technology.

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Kontaktid Ajakirjanduse jaoks

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com