Lehdistötiedote

Siemens introduces a new type of motor starter

14. marraskuuta 2024
Hungary

Featuring semiconductor technology, the device is more durable and up to 1,000 times faster than conventional alternatives.

Industries such as food and beverage production, intralogistics and mechanical engineering rely on powerful motors to drive conveyor belts and start machinery. Motor failures can cause significant damage, making motor starters, which control the power supplied to these motors, essential components in industrial facilities. They must also provide protection against overloads and short circuits. In the food industry, where strict hygiene requirements mean conveyor systems frequently need to be cleaned using high-pressure washing, water can easily cause short circuits, resulting in costly downtime.

To help prevent such incidents, Siemens has introduced the new SIMATIC ET 200SP e-Starter, which detects short-circuit currents up to 1,000 times faster than conventional solutions and disconnects equipment within just 4 µs (microseconds) in the event of a fault. This ultra-fast, virtually wear-free switching – compared with conventional circuit breakers or fuses – is made possible by the use of semiconductor technology featuring silicon carbide metal-oxide-semiconductor field-effect transistors (SiC MOSFETs).

2 Illusztracio Elelmiszeripar

Once the cause of the short circuit has been eliminated, the device can be restarted immediately and supports an unlimited number of short-circuit disconnections. Unlike conventional solutions, there is no need to replace the device or obtain spare parts, helping to increase plant availability.

The compact, easy-to-install device features integrated diagnostic functions and is compatible with Siemens’ Totally Integrated Automation (TIA) engineering environment. It has also received the Siemens EcoTech label, the company’s sustainability designation for its most environmentally responsible solutions. The motor starter earned this recognition for its reduced material consumption, energy efficiency and durability.

The new motor starter is also available on the Hungarian market.

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Yhteystiedot lehdistölle

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com