Communiqué de presse

New solutions in industrial switchgear technology

20 avril 2026
Hungary

SIRIUS 3RF5

The SENTRON 3QD2 solid-state circuit breaker and the SIRIUS 3RF5 switchgear are now available for DC applications.

Siemens’ new solutions address the growing demands of industrial switching technology. The newly launched solid-state circuit breaker, based on intelligent protection algorithms, is capable of interrupting short circuits in the microsecond range—up to a thousand times faster than conventional systems. This is essential for the operation of direct current (DC) networks and significantly increases the level of protection as well as system availability.

The compact, multifunctional, configurable SENTRON 3QD2 combines protection, switching, monitoring, and energy management functions, replacing multiple separate devices and providing significant space savings. Thanks to its maintenance-free design and the absence of mechanical wear parts, it guarantees a long service life and maximum operational reliability, making it ideal for use in critical infrastructure applications.

SENTRON 3QD2 semiconductor cirucit breaker (SCCB)

SENTRON 3QD2

This device is complemented by the SIRIUS 3RF5 solid-state switch (relay), which has no moving parts and uses semiconductors to control circuits, making it the first solution of its kind for DC applications. Designed specifically for high-frequency switching of resistive loads, it offers a low-wear, durable solution that increases the efficiency and availability of industrial equipment.

The SIRIUS 3RF5 device is also being launched with the Siemens EcoTech certification, which signifies sustainability.

First unveiled at the Hannover Messe 2026 industrial trade show, these solutions—which can be integrated into SIVACON S8 low-voltage switchgear or SIVACON 8PS busbar systems—will serve in facilities requiring high power.

SENTRON 3QD2 megszakító - ultragyors reakció

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Contacts presse

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com