Communiqué de presse

Siemens launches SIMATIC AX WinCC Unified Elements

28 juillet 2026
Alpharetta, GA, USA

  • New IT-style engineering tool speeds automation application development, reducing the time required to bring industrial projects to market.

Siemens—a global leader in industrial AI and automation technology—announced the launch of SIMATIC AX WinCC Unified Elements, an IT-like engineering application for the SIMATIC WinCC Unified system. This application empowers automation engineers to build, perform version control, and deploy visualization engineering projects with the same workflows used by IT software developers. The application is available now exclusively in the United States, giving manufacturers an opportunity to bring modern software practices to the plant floor.

The manufacturing industry faces a widening gap between the pace of digital transformation and the availability of skilled automation talent. As product development and change cycles shrink while the need for efficiency grows, a new generation of IT-minded engineers expects modern software development tools that move beyond traditional engineering ecosystems. SIMATIC AX WinCC Unified Elements addresses this gap with an open, code-based engineering environment for visualization that runs alongside traditional graphical, drag-and-drop editor-based workflows.

Key innovations for accelerated development include:

Full project generation from human-readable YAML files – at the software’s core, the application empowers engineers to build complete automation projects, combining AI-generated code, configurations, scripts, and reusable library packages into a ready-to-deploy build.

Seamless hybrid workflows – embedded hybrid workflows facilitate working simultaneously with both graphical development environments and direct code editing, responsive to each other in real time.

Open architecture – users can run custom web controls in the same environment, with no external APIs required.

Enhanced collaboration – native Git integration provides full project history, branching, and merge-request workflows for visualization project development to support coworking in real time among distributed teams. The extension-based IDE—built on the Open VSX marketplace—provides customization capabilities so engineers can tailor the development environment to their needs and receive new features as background updates, with no forced upgrades or added licensing cost.

“We're witnessing a fundamental shift in industrial automation, where the speed of innovation is no longer limited by engineering tools but enabled by them,” says Adrien Amar, Global Business Development Manager, Software Defined Automation and SIMATIC AX WinCC Unified Elements at Siemens Digital Industries. “For decades, we've helped manufacturers automate their production lines; now we're automating the automation itself. With SIMATIC AX WinCC Unified Elements, engineers can generate, validate, and deploy automation projects at software speed—using AI generation, CI/CD pipelines, and the version control that IT teams have relied on for years.”

"The US release of SIMATIC AX WinCC Unified Elements marks an important step forward in modernizing industrial engineering workflows, bringing visualization and control engineering together in a unified development environment,” adds Cory Rinaldi, Portfolio Sales Enablement Manager, SCADA & Edge, North America, Siemens. “By combining visual and text-based engineering, native Git integration, and AI-ready workflows, we're helping customers accelerate development, improve collaboration, and adopt IT-driven engineering practices without compromising the reliability expected in industrial automation. Initially supporting WinCC Unified PC Runtime applications, WinCC Unified Elements provides customers with a modern engineering approach, while expanding the flexibility and choices available within the Siemens automation portfolio.”

SIMATIC AX WinCC Unified Elements extends the SIMATIC AX family—which previously focused solely on PLC programming—into visualization, providing engineers with a single, IT-aligned environment to develop both control logic and its interfaces.

To learn more about SIMATIC AX WinCC Unified Elements or to start a free trial, contact your Siemens representative, or visit www.siemens.com/unified-elements/.

Siemens Digital Industries (DI) permet aux entreprises de toute taille des secteurs de la fabrication par procédés et de la fabrication discrète d’accélérer leur transformation en entreprises numériques et écoresponsables dans l’ensemble de leur chaîne de valeur. Le portefeuille de solutions d’automatisation et de logiciels de pointe de Siemens révolutionne la conception, la réalisation et l’optimisation des produits et de la production. Et avec Siemens Xcelerator – la plateforme d’entreprise numérique ouverte – ce processus est encore plus facile, plus rapide et plus évolutif. En collaboration avec ses partenaires et son écosystème, Siemens Digital Industries permet à ses clients de devenir des entreprises numériques écoresponsables. Siemens Digital Industries emploie environ 70 000 personnes à travers le monde.

Contacts presse

Karen Kasik
Siemens Digital Industries
Media Relations Manager
Phone: +1-470-709-3641
Email: karen.kasik@siemens.com