Communiqué de presse

What comes after the gigafactories?

15 juin 2026
Hungary

The manufacturing process at Haddy's microfactory.

Microfactories do not produce excess inventory.

The vulnerability of global supply chains and increasingly stringent sustainability requirements are also placing new demands on the manufacturing sector: mass-production factories, which have been in operation for over a century, now face new competition from highly automated microfactories that are tailored to individual needs, operate locally, and are situated in close proximity to consumer markets.

These small businesses and family-run workshops—essentially reimagined using Industry 4.0 technology—represent a new trend in sustainable manufacturing; by 2025, they already accounted for a $6 billion global market, and this is expected to nearly triple by 2030.

Small, Green, and Efficient

Microfactories are small- or medium-sized, technologically advanced, and automated manufacturing units that are not set up for mass production, yet are highly scalable and offer broad capacity flexibility. Although the concept dates back several decades, its commercial-scale application has only been made possible by the widespread adoption of industrial robots, artificial intelligence, and IoT applications.

Microfactories require radically fewer resources: the size of equipment and systems is directly tailored to the characteristics, shape, and packability of the end product, thereby reducing the factory’s floor space—and with it, the required capital investment and operating costs. For example, while a microfactory overseas can be launched with as little as $50,000, a traditional factory typically starts in the range of several million dollars.

siemens-haddy-newsroom-04-1280x720

Actual production typically begins here once the manufacturer receives a confirmed or prepaid advance order. With this approach, the market is not burdened with excess inventory (push strategy); instead, production is driven by actual consumer demand and organized according to a so-called pull strategy.

This is not only a more sustainable model, but consumer demand is also moving in this direction: according to surveys, more than half of the population in developed countries explicitly prefers personalized products and is willing to pay a higher price for them. Microfactories, meanwhile, can switch designs at minimal cost or even for free, meaning that small-batch, custom orders can be fulfilled immediately and without loss.

One example is the increasingly popular “slow fashion” sector, which—instead of the mass-produced goods of the “fast fashion” clothing industry shipped from far away—manufactures every single item tailored directly to the user’s needs, even based on an order placed via a smartphone.

Local production instead of complex logistics and massive warehouses

In the traditional manufacturing model, production is outsourced to distant regions—primarily Asia or Eastern Europe—due to cheaper labor. However, this requires a long supply chain, warehouse networks, and continuous restocking. Maintaining this distribution network is very costly for a traditional factory, accounting for about 25–40 percent of the product’s final production cost.

In contrast, for microfactories focused on the local market, this figure is only 5–10 percent, meaning that significant savings on logistics costs can be achieved even if the fixed cost per product is higher due to small-batch production.

Five Flexbots in a row at the microfactory

Furthermore, this approach eliminates tied-up inventory and eliminates the need to maintain massive warehouses, while manufacturing facilities can also serve as showrooms and sales outlets. This flexibility makes businesses resilient to disruptions in global supply chains or new waves of international tariffs. Furthermore, in developing countries, younger generations are increasingly unwilling to work in monotonous, low-skilled jobs, leading to rising wages and labor shortages at large factories.

Software-Controlled Manufacturing

The competitiveness and scalability of microfactories are underpinned by standardized, software-controlled manufacturing processes that span the entire end-to-end value chain—from design all the way through to sales. These highly digitized systems, which integrate AI and robotic solutions, can be replicated anywhere in the world. Thanks to AI-based digital twins and cloud-based manufacturing software, they can operate with minimal IT infrastructure yet with engineering precision, and they optimize themselves through continuous data collection.

This is how Haddy, for example, operates in the United States, manufacturing components—such as furniture—from recyclable materials in digitally standardized, AI-supported microfactories.

The company uses software available on the Siemens Xcelerator open digital business platform to design and prepare parts for robotic manufacturing; it uses this software to manage robot-controlled material forming and CNC machining processes, and it also receives support for product optimization and the development of manufacturing strategies and simulations.

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Contacts presse

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com