Comunicato stampa

New SINAMICS S210 next generation servo-drive system upgrades mid-range product portfolio

24 maggio 2023

  • 1AC 230V, 50–750W and 3AC 200-480V, 0.4–7kW versions
  • Digitally native drive system from planning to operations
  • Security Chip Integration and UMAC program protection
  • PROFIsafe integrated SIL3 / PLe safety functionality
  • Combines with PLC via technology object for advanced motion control
  • 3C3 and ANSI/ISA G3 compliant coating for harsh environments
  • Motor options available for numerous manufacturing industries

With the SINAMICS S210 next generation servo-drive system, comprising a digitally native drive with wide range of corresponding motors and gearboxes, Siemens brings a new level of high-dynamic, motion control in mid-range operation to stand-alone and multi-axis machines. It will be introduced to the North American manufacturing industry during AUTOMATE 2023.

This next generation servo-drive system introduces a new level of safety and security to discontinuous motion control in the mid-range segment, as well as moving, processing and positioning functions on a wide assortment of packaging, printing, labeling, pick-and-place, stacking, assembly, chip sorting and filling machines, with a special emphasis on food-and-beverage and pharmaceutical applications, owing to the availability of stainless-steel motor and planetary gearbox options.

SINAMICS S210 offers DC link coupling on 3-phase units for increased power efficiency on multi-axis applications. Corresponding SIMOTICS highly efficient synchronous motors feature high-resolution 22- or 26-bit absolute encoders, single or multi-turn. One-cable connectivity is standard and all motors and feature IP64, IP65, IP67 or IP69X protection. Easier setup and selection are assured with the integrated EMC filter and braking resistor.

For the engineering of SINAMICS S210, machine builders and machine users can utilize the embedded web-server or Startdrive integrated with the Siemens TIA Portal. Easy implementation of the SINAMICS S210 servo-drive system for global use is provided by universal standards and certification compliance.

SINAMICS DriveSim model integrates into simulation software to allow machine builders to create a digital twin of the drive and motor in a project’s planning phase to ensure highest efficiency and performance of the equipment in use. In the field, the S210 is capable of communicating status through Edge or cloud-based data capturing for continuous monitoring and data analytics. Using the Siemens Analyze MyDrives application, machine users can monitor key conditions for advanced anomaly detection. Seamless transfer of data from the drive to the machine controller, Edge device and the cloud are maintained for truly digital native operation from planning through operations.

In the area of cybersecurity, SINAMICS S210 comes standard with integrated security for network connectivity, providing enhanced communication, integrity and authenticity checks to protect against tampering, plus the drives offer User Management and Access Control (UMAC) within TIA Portal.

These new servo-drives are paired with the popular Siemens SIMATIC S7-1500 PLC or ET200 SP open controller and various SIMOTICS servomotor and planetary gearbox designs. Increased engineering efficiencies are gained with integration into the TIA Portal and TIA Selection Tool for optimized system selection and programming.

With Safety Integrated onboard, the SINAMICS S210 servo-drive system offers machine users up to SIL3 level of protection across an extended range of safety integrated functions including safe stopping and safe limited speed or direction. Integrated into the Startdrive advanced software, the menu-guided safety acceptance testing assures proper operation and safety validation.

The new SINAMICS S210 next generation servo-drive system is ready for digitalization and brings an enhanced level of safety and security to stand-alone or multi-axis machines for use in various manufacturing industries.

Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.

Siemens Corporation is a U.S. subsidiary of Siemens AG, a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power. In fiscal 2022, which ended on September 30, 2022, Siemens Group USA generated revenue of $18.6 billion and employs approximately 45,000 people serving customers in all 50 states and Puerto Rico.

Contatti per la stampa