보도 자료

SAICEC and Siemens to accelerate chip-to-vehicle validation using digital twin technology

2025년 11월 17일
Plano, Texas, USA

SAICEC, a leading provider of chip and system design services for the automotive industry, has begun building complex digital twins of automotive architectures based on Siemens’ PAVE360 software (Image credit: SAICEC)
  • SAICEC creating digital twins of its automotive systems with Siemens’ PAVE360 to enable certified system-to-chip level verification and accelerate software defined vehicle (SDV) development in Asia
  • The collaboration helps OEMs address Advanced Driver Assistance Systems (ADAS) and In-Vehicle Infotainment (IVI) development challenges by enabling early validation and reducing costly redesigns
  • PAVE360 provides a scalable digital environment that supports faster innovation, improved safety and reduced development timelines

Today, Siemens announced that SAICEC, a leading provider of chip and system design services for the automotive industry, has begun building complex digital twins of automotive architectures based on Siemens’ PAVE360™ software, facilitating comprehensive verification of automotive components from system-level to chip-level.

This initiative will accelerate the adoption of advanced solutions that help overcome the challenges of software-defined vehicle (SDV) development. It also supports OEMs in identifying next-generation chip technologies and developing critical systems at the scale and speed demanded by the mobility industry.

“Our collaboration with Siemens brings together world-class simulation technology and China’s fast-growing automotive integrated circuit (IC) ecosystem,” said David He, chief executive officer, SAICEC. “With Siemens’ PAVE360 system-to-chip digital twin capabilities, we can shorten development cycles, improve functional safety and strengthen the foundation for intelligent mobility design."

“Our work with SAICEC demonstrates how automotive OEMs are able to solve critical bottlenecks in ADAS and IVI capabilities development and deliver the innovation that consumers across the globe are demanding,” said Mike Ellow, CEO, Siemens EDA, Siemens Digital Industries Software. “PAVE360 is uniquely placed to provide the digital twin to support SAICEC’s new validation certification. With scalability at its core, the same multi-fidelity environment can be adapted over time to provide validation throughout the entire vehicle development flow.”

SDV programs grow in complexity as consumer expectations for integrated technology also continue to increase. Today’s automotive hardware and software teams often operate in silos across disparate environments, with limited access to a system-level view until final hardware is available. This lack of early-stage validation leads to costly redesigns when final hardware fails certification tests. System-level verification before hardware availability is now essential for future success.

PAVE360 leverages Siemens’ Innexis™ software environment combined with supporting technologies to empower users to create system-level digital twins of ADAS and IVI capabilities. These digital twins can be connected to reference vehicles to perform functional validation from the earliest design stages. OEMs and suppliers alike can leverage PAVE360 to accelerate validation and foster innovation within a proven, real-world digital environment.

To learn more about how Siemens’ PAVE360 is helping customers like SAICEC reduce vehicle development timelines, visit https://eda.sw.siemens.com/en-US/pave360/

지멘스 디지털 인더스트리 소프트웨어 소개

지멘스 디지털 인더스트리 소프트웨어는 규모에 상관없이 모든 기업들이 Siemens Xcelerator 비즈니스 플랫폼의 소프트웨어, 하드웨어, 서비스를 사용해 디지털 전환을 추진하도록 지원한다. 지멘스의 소프트웨어와 포괄적인 디지털 트윈을 통해 기업은 설계, 엔지니어링, 제조 프로세스를 최적화함으로써 오늘의 아이디어를 미래의 지속가능한 제품으로 만들어낼 수 있다. 칩부터 전체 시스템까지, 제품부터 프로세스까지, 모든 산업을 아우른다.Siemens Digital Industries Software – Accelerating transformation.

지멘스 관련 상표 목록은 여기에서 찾아볼 수 있다. 기타 상표는 해당 소유자에게 속한다.

언론 연락처