보도 자료

Siemens’ breakthrough Veloce CS transforms emulation and prototyping with three novel products

2024년 2월 20일
Plano, Texas, USA

Siemens' Veloce CS system pictured as single blades (from top) Veloce Strato CS for emulation, Veloce Primo CS for enterprise prototyping, and Veloce proFPGA CS for software prototyping.
  • Innovative Veloce CS architecture unifies hardware emulation, enterprise prototyping and software prototyping to accelerate verification and validation cycles by 10x and helps to reduce total cost of ownership by up to 5x
  • The Veloce CS software is reusable across all platforms, helping to eliminate new learning requirements and accelerating full system workload execution and debug times by 10x
  • Innovative, modular and scalable interconnectable blade footprint eliminates fixed-size chassis, delivering hardware-assisted tools for all size designs – from small to very large

Siemens Digital Industries Software launched today the Veloce™ CS hardware-assisted verification and validation system. In a first for the EDA (Electronic Design Automation) industry, Veloce CS incorporates hardware emulation, enterprise prototyping and software prototyping and is built on two highly advanced integrated circuits (ICs) – Siemens’ new, purpose-built Crystal accelerator chip for emulation and the AMD Versal™ Premium VP1902 FPGA adaptive SoC (System-on-a-chip) for enterprise and software prototyping.

The solution encompasses three new offerings:

  • Veloce™ Strato CS hardware for emulation.
  • Veloce™ Primo CS hardware for enterprise prototyping.
  • Veloce™ proFPGA CS hardware for software prototyping.

Architected for congruency, speed, and modularity across all three platforms, the Veloce CS system supports design sizes from 40 million gates, up to designs integrating more than 40+ billion gates. In addition, Veloce CS executes full system workloads with superior visibility and congruency by selecting the right tool for the task, as each task has unique requirements. This enables much faster time to project completion and assists in decreasing cost per verification cycle.

To achieve this milestone, Siemens has worked with key customers and partners to develop innovative hardware and a new, fully unified software architecture:

  • Veloce Strato CS delivers significant emulation performance improvement over Veloce Strato, up to 5x maintaining full visibility and it scales from 40 million gates (MG) to 40+ billion gates (BG).
  • Veloce Primo CS, based on AMD’s latest Versal Premium VP1902 FPGA, is the industry’s most congruent enterprise prototyping system, and it also scales from 40MG to 40+BG.
  • Both the Veloce Strato CS and Veloce Primo CS solutions run on the same operating system, which delivers exceptional congruency while providing the freedom to seamlessly move between platforms. This can dramatically accelerate ramp up, setup time, debug, and workload execution.
  • Veloce proFPGA CS, which also leverages the AMD Versal Premium VP1902 FPGA-based adaptive SoC, which delivers a fast and comprehensive software prototyping solution, scaling from one FPGA to hundreds. This exceptional performance, together with its highly flexible and modular design, can help customers dramatically accelerate firmware, operating system, application development and system integration tasks.

The entire Veloce CS system is available in a modular blade configuration that is fully compliant with modern datacenter requirements for easy installation, low power, superior cooling, and compact footprints. Further, the Veloce proFPGA CS solution provides a desktop lab version for additional user flexibility.

Veloce CS is qualified to run with the latest AMD EPYC™ CPU-powered HP DL385g11 servers.

“The evolution of SoC and system level design has brought about many changes in the last ten years that have made the use of hardware-assisted verification more necessary than ever,” said Alex Starr, Corporate Fellow, AMD. “We have been working closely with Siemens to incorporate AMD’s leading Versal Premium VP1902 device into the heart of the Veloce Primo CS and Veloce proFPGA CS systems for increased performance and scalability, as well as qualifying the AMD EPYC CPU-powered HP DL385 gen11 servers for use with the entire Veloce CS system. The Veloce CS system, including the Veloce Strato CS emulation platform, shows how Siemens responds to customer needs and showcases the innovation happening in the Veloce group.”

Customers have access to the industry’s most comprehensive portfolio of apps and solutions, common across all three new Veloce CS system offerings.

“Time to market is critical to the entire Arm partner ecosystem, emphasizing a need for tools that offer modularity, granularity and speed for IP and SoC verification,” said Tran Nguyen, senior director of design services, Arm. “Siemens’ Veloce platforms have become an integral part of the Arm development process and we continue to see benefits of the new Veloce Strato CS system for hardware design acceleration and software development.”

“Veloce CS provides the industry’s only fully congruent, high-speed, modular hardware-assisted system with three systems,” said Jean-Marie Brunet, vice president and general manager, Hardware-Assisted Verification, Siemens Digital Industries Software. “With the Veloce CS system, we are addressing the specific needs of hardware, software, and system engineers who all play an essential part in delivering the world’s most advanced electronic products. By providing the right tool for the task, Veloce CS innovations speed up the entire verification process, and lower total cost of ownership, which can boost profitability.”

Availability

The Veloce Strato CS system is available now for selected partner customers. General availability of the three hardware platforms is planned for summer 2024. The Veloce CS system is planned to be cloud ready with general availability. To learn more about how Siemens is enabling the semiconductor and electronic systems industry to deliver to market the world’s most advanced SoCs and systems, visit: https://eda.sw.siemens.com

지멘스 디지털 인더스트리 소프트웨어 소개

지멘스 디지털 인더스트리 소프트웨어는 규모에 상관없이 모든 기업들이 Siemens Xcelerator 비즈니스 플랫폼의 소프트웨어, 하드웨어, 서비스를 사용해 디지털 전환을 추진하도록 지원한다. 지멘스의 소프트웨어와 포괄적인 디지털 트윈을 통해 기업은 설계, 엔지니어링, 제조 프로세스를 최적화함으로써 오늘의 아이디어를 미래의 지속가능한 제품으로 만들어낼 수 있다. 칩부터 전체 시스템까지, 제품부터 프로세스까지, 모든 산업을 아우른다.Siemens Digital Industries Software – Accelerating transformation.

지멘스디지털인더스트리(Siemens Digital Industries, DI)는자동화및디지털화분야의혁신리더이다. DI는파트너및고객사와긴밀히협력해프로세스및개별산업의디지털혁신을추진하고있다. DI는디지털엔터프라이즈포트폴리오를통해다양한규모의기업에엔드-투-엔드제품과솔루션, 서비스를제공해전체가치사슬을통합하고디지털화한다. 각산업의개별요구사항에최적화된 DI 고유의포트폴리오는고객이생산성과유연성을확대할수있도록지원한다. DI는최첨단기술을통합하기위해자체포트폴리오를지속적으로혁신하고있다. 지멘스디지털인더스트리의글로벌본사는독일뉘른베르크에위치해있으며, 전세계에약 7만 6,000명의직원을두고있다.

지멘스 소개 

독일 베를린과 뮌헨에 본사를 둔 지멘스는 산업, 인프라, 운송, 헬스케어 등의 분야에 역량을 집중하고 있는 세계적인 기술 기업이다. 공장의 자원 효율성 개선, 탄력적인 공급망 관리, 스마트 빌딩 및 그리드는 물론, 보다 친환경적이고 편리한 운송 서비스와 첨단 헬스케어 서비스 분야에 이르기까지 지멘스의 기술은 고객을 위한 진정한 가치를 창출하는 데에 그 목적을 둔다. 지멘스는 현실과 디지털 세계를 결합함으로써 고객이 산업과 시장을 변화시키고 더 나아가 수십억 인구의 일상을 변화시킬 수 있도록 지원한다. 지멘스는 헬스케어 산업의 미래를 견인하고 있는 세계적 의료기술 기업이자 상장 계열사인 지멘스 헬시니어스의 최대 지분을 보유하고 있다. 

2023년 9월 30일 종료된 2023 회계연도에 지멘스 그룹의 매출액은 778억 유로, 순이익은 85억 유로다. 2023년 9월 30일 기준 전 세계적으로 32만 명의 직원이 근무하고 있다. 자세한 내용은 www.siemens.com에서 확인할 수 있다. 

지멘스 관련 상표 목록은 여기에서 찾아볼 수 있다. 기타 상표는 해당 소유자에게 속한다.

언론 연락처