Pranešimas Spaudai

Altair acquires Flow Simulator; an integrated flow, heat transfer, and combustion design software, from GE Aviation, to expand into new industries

2021 m. vasario 24 d.
Troy, Michigan, USA

  • Altair and GE Aviation establish strategic engagement to pursue new opportunities

Altair, a global technology company providing software and cloud solutions in the areas of simulation, high-performance computing (HPC), and artificial intelligence (AI), today announced that it has acquired Flow Simulator from GE Aviation. Flow Simulator is an integrated flow, heat transfer, and combustion design software, which enables mixed fidelity simulations to optimize machine and systems design.

As part of the acquisition, Altair and GE Aviation have signed a memo of understanding (MOU) to facilitate a higher level of collaboration and establish a long-term strategic partnership. The relationship will include Altair’s continuous development of Flow Simulator; granting GE Aviation access to Altair’s complete software suite to explore enhanced functionality aligned to real-world use cases and workflows; and ongoing executive engagement between both parties to establish deeper strategic alignment and pursue new ventures.

altair-acquires-flow-simulator-flow-heat-transfer-combustion-design-software-from-ge-aviation-body-image 01

“We successfully collaborated with GE Aviation for many years on several initiatives including rotor dynamics using Altair OptiStruct, which opened doors for new opportunities to work together. We value our strong relationship with GE Aviation as we join forces to drive innovation for aircraft engines and beyond,” said James R. Scapa, founder and chief executive officer, Altair. “Utilizing Altair's simulation and AI-driven approach to innovation, there is great potential to expand Flow Simulator’s capabilities and make it available to new industries focused on simulating systems models including automotive, electromobility, battery, defense, and renewable energy.”

“Altair will bring Flow Simulator’s capability to simplify the modeling of complex thermal systems to new industries. This will expand global technical capabilities,” explains Arjan Hegeman, senior executive – Technology, GE Aviation. “Concurrently, GE Aviation and Altair will continue developing Flow Simulator together, with even more advanced simulation technologies and design tools that will continue to expand its capabilities for a broader base of users.”

System-level design has become increasingly critical as organizations are tasked with simulating complex duty cycles. Fast software solutions like Flow Simulator are needed to model an entire system, including rapid iteration concept modeling and understanding of system simulation and system behavior in applications such as rotating machinery design, electromobility, wind turbines, heat exchangers, and virtually anything that encompasses thermal management.

GE Aviation developed Flow Simulator to serve as a fast flow network simulator for aircraft engines – simulating how an entire flight cycle would behave in the real world, from runway and take off to flight and landing. Since its inception, it has been used to simplify modeling for a variety of complex thermal systems applications, including healthcare, locomotives, and renewable energy. Prior to acquiring the technology, Altair was a commercial distributor of Flow Simulator, which was available through the Altair Partner Alliance (APA).

altair-acquires-flow-simulator-flow-heat-transfer-combustion-design-software-from-ge-aviation-body-image 02

Key features of Flow Simulator include:

  • Fully-coupled flow/thermal network modeling – An extended library of preconfigured elements and components leveraging a large set of publicly-available experimental data for pressure drop and heat transfer characteristics.
  • Control system module – Proportional integral derivative (PID) controllers, feedforward, and missions can be integrated with flow/heat transfer models to optimize the simulated-machine operation during cycle/mission analysis.
  • Optimization module – Monte Carlo, Optimal Latin Hypercube, and N-factorial analyses quickly explore the entire design space of a 3D modeling environment. An analytical model can be parametrized based on flow configuration, shape, dimension, and thermal characteristics to achieve an optimal cost-benefit design.
  • User-defined elements – Ability to integrate a customer's own IP and element formulations using UDE creator supported in flexible python scripting as well as with Fortran language. APIs are provided an option to connect Flow Simulator with external software for multidisciplinary analyses.
  • Intuitive interface – A modern interface for pre, post, solve, and optimization. The three-dimensional design environment gives users the ability to overlay/integrate the network model with 3D computer-aided design (CAD) while integrating a customer’s IP and element formulations seamlessly.

For more information about Flow Simulator, visit https://www.altair.com/flow-simulator/.

Altair is a global leader in computational intelligence that provides software and cloud solutions in simulation, high-performance computing (HPC), data analytics, and AI. Altair is part of Siemens Digital Industries Software. To learn more, please visit altair.com or sw.siemens.com.

About GE Aviation

GE Aviation, an operating unit of GE (NYSE: GE), is a world-leading provider of jet and turboprop engines, components, integrated digital, avionics, electrical power and mechanical systems for commercial, military, business and general aviation aircraft. GE Aviation has a global service network to support these offerings and is part of the world's Digital Industrial Company with software-defined machines and solutions that are connected, responsive and predictive. For more information, visit us at https://www.ge.com/aviation. Follow GE Aviation on Twitter at https://twitter.com/GEAviation and YouTube at https://www.youtube.com/user/GEAviation.

Kontaktai Spaudai

Siemens Digital Industries Software PR Team

Email: press.software.sisw@siemens.com