Pranešimas Spaudai

Siemens launches Eigen Engineering Agent in Thailand, bringing purpose-built industrial AI to automation engineering

2026 m. rugpjūčio 27 d.
Bangkok, Thailand

  • Siemens today introduces the Eigen Engineering Agent, its purpose-built Industrial AI for automation engineering, to Thailand for the first time
  • The Thailand launch includes the agent's capabilities available globally today, from programmable logic controller (PLC) coding, human-machine interface (HMI) visualization and device configuration to ECAD integration and standards-compliant project generation
  • Globally, the Eigen Engineering Agent is already used by more than 100 companies in 19 countries, completing engineering workflows 2 to 5 times faster than manual methods, with up to 80 percent higher solution quality and 50 percent greater engineering efficiency

Siemens today launched the Eigen Engineering Agent in Thailand, bringing its purpose-built industrial AI for automation engineering to the Thai market for the first time. The Eigen Engineering Agent moves AI beyond on-screen suggestions to action in the physical world and is now available to automation engineers across Thailand with its complete set of capabilities.

Industrial AI that acts, not just advises

Most AI assistants generate suggestions that engineers must still translate into their own projects. The Eigen Engineering Agent does the work itself: it plans, executes and validates automation engineering tasks end-to-end. It understands the project, writes the control software, configures the system and keeps refining its work until it meets defined quality benchmarks, freeing automation engineers to focus on system-level decisions.

The Eigen Engineering Agent works alongside TIA Portal, Siemens' engineering software platform, and is part of the Siemens Xcelerator portfolio. Because it connects directly to TIA Portal, it has full awareness of a project's data structures, blocks, parameters and component relationships, allowing it to deliver outputs tailored to what engineers are actually building, including on legacy or undocumented systems.

From electrical design to a standards-compliant project, in one workflow

Thai customers adopting the Eigen Engineering Agent gain access to its complete range of capabilities from day one. Beyond core tasks such as PLC coding, HMI visualization and device configuration, this includes two capabilities that extend the agent further upstream in the engineering lifecycle:

  • ECAD integration: the agent reads electrical design files in widely used formats including XML and AML, detects inconsistencies, resolves or flags them, adds devices to the TIA Portal project, configures the connections and generates PLC tags grounded in the actual hardware topology, closing the gap between electrical design and automation code.
  • Standards-compliant project generation: engineers describe a machine in plain language, its stations, devices and how it should behave and the agent generates a complete project that follows the Siemens Automation Framework, Siemens' best-practice reference for structuring TIA Portal projects, ready to open and build on directly in TIA Portal.

Addressing Thailand's automation engineering talent gap

As Thai manufacturers face tightening innovation cycles and a persistent shortage of skilled automation engineers, the Eigen Engineering Agent is designed to free engineers to focus on higher-level system challenges without compromising accuracy or reliability.

Productivity gains in the real world

Since its global launch, the Eigen Engineering Agent has been adopted by more than 100 companies in 19 countries, including ANDRITZ Metals (Austria), CASMT (China) and Prism Systems (United States). The agent accelerates everyday engineering work such as PLC programming, HMI visualization and device configuration, with measurable gains:

  • 2 to 5 times faster execution than manual workflows
  • Up to 50 percent efficiency gains in engineering
  • 80 percent improvement in overall solution quality

Onboarding has also improved: at one automotive line builder, new engineers who previously spent weeks learning a project's structure could instead query it directly, cutting onboarding time from weeks to days.

The Eigen Engineering Agent, including the ECAD integration and standards-compliant project generation capabilities, is available now to customers in Thailand as part of the standard subscription.

Live at NECTEC ACE 2026

The Eigen Engineering Agent will be among the highlights at the Siemens booth during NECTEC ACE 2026 at Paragon Hall, Siam Paragon, Bangkok on September 3, 2026, shown alongside highlights from Siemens' industrial AI portfolio:

  • AI-Powered Engineering & Automation
    Eigen Engineering Agent: Generative AI-powered assistant for automation engineering, connected to TIA Portal, helping engineers accelerate project creation, code development, testing, and system configuration
  • AI-Driven Digital Twin & Simulation
    Digital Twin Composer:Siemens’ comprehensive digital twin technology that combines high-fidelity 2D and 3D digital twins with real-time operational data, enabling organizations to design, simulate, test, and optimize products, production systems, and industrial operations in a virtual environment before implementation in the real world.
  • Industrial AI Analytics & Decision Intelligence
    Rapidminer:Siemens’ enterprise AI and analytics platform that unifies data preparation, machine learning, knowledge graphs, generative AI, and agentic AI to help organizations transform complex operational data into actionable insights.

Those interested in seeing these technologies in action are welcome to visit the Siemens booth at NECTEC ACE 2026 for live demonstrations.

About Siemens

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Kontaktai Spaudai

Siemens Limited
Corporate Communications
Email: cm.th@siemens.com