Pranešimas Spaudai

These devices support the operation of an environmentally friendly smart hall

2025 m. birželio 3 d.
Hungary

Source: Weerts Logistics Park

Comfort automation, control, and drive technology solutions in the new production hall built in the Weerts Logistics Park in Vecsés.

Sustainability and good neighborly relations received particular attention during the development of one of Hungary’s newest production halls, which was handed over in October 2024. At the Vecsés site of Weerts Logistics Park, one of the world’s largest automotive parts suppliers built a 40,000-square-meter smart hall, which is expected to supply local car factories with body components from the end of 2025, while the office section will provide workplaces for several hundred employees.

At the new site, in the spirit of cooperation with the local community, a humus mound planted with trees and shrubs is responsible for noise filtering, solar panels installed on the roof will partly provide the electricity supply, and the plant will also reuse rainwater and the waste heat generated by the machines.

Systems that enable weather-dependent and value-maintaining control of the heat demand of the building and the production technology also contribute to environmentally friendly operation. These are responsible, for example, for continuously maintaining the temperature of hot water in storage tanks or for adjusting the temperature of the water used for heating depending on whether the outside temperature is currently +30°C or -10°C.

For these systems, Siemens Zrt., through its partner Galik Energetika Kft., supplied nearly fifty large motorized control and butterfly valves suitable for high-power consumers, enabling heat center and zone control. In the production hall, the technology company’s control and drive systems are also used, while Siemens HMI (human-machine interface) operator panels and switches will ensure the smooth control of the technology and automation used for production.

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Kontaktai Spaudai

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com