Pranešimas Spaudai

Introducing the new generation of logic controllers

2026 m. kovo 11 d.
Hungary

LOGO! 9 promises greater performance and security.

Siemens has unveiled a new-generation, entry-level automation controller. The LOGO! controller, revamped after 11 years, promises simple implementation of smaller automation projects—such as stairwell lighting automation, low-voltage electrical switching automation, booster pump control, or machine manufacturing.

“What could previously be achieved with simple logic functions now requires precise data processing, intuitive operating concepts, and comprehensive security. Available on the domestic market starting in April, LOGO! 9 combines the computing power and security standards of larger systems with the simplicity and cost-effectiveness of compact logic modules,” – emphasized Zsolt Barabás, an expert at Siemens Zrt.

Enhanced capabilities for everyday use

LOGO! 9 offers twice the number of function blocks, up to 800, so in many cases there is no need for additional control devices. The previous push-button design has been replaced by a touchscreen color display, which is now available in a larger size for users. The range of secondary (TDE) displays has also been updated and is now available in a 4.3-inch size, allowing LOGO! data to be displayed on the front panel of the control cabinet.

The new device’s software can be loaded from a USB flash drive as a Plug & Play solution and is fully compatible with previous projects and generations. Together with the integrated LOGO! Web Editor simulation, it is a cross-platform tool that now supports macOS and Linux systems in addition to Windows. The new user management system ensures access control through four user roles.

LOGO! 9 carries the Siemens EcoTech label, meaning it meets the technology company’s highest sustainability standards. Secure Boot and secure LOGO! communication provide protection against unwanted manipulation and unauthorized access. Firmware updates via LSC (LOGO! Soft Comfort) and factory reset with IP address retention ensure safe and efficient operation throughout the entire lifecycle.

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Kontaktai Spaudai

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com