Pranešimas Spaudai

Fontos gáztároló folyamatos működését biztosítja Siemens-technológia

2024 m. lapkričio 5 d.
Hungary

Source: MFGT

Image source: MFGT

Low-voltage electrical equipment supporting the cooling systems at the Zsana natural gas storage facility has been expanded.

The four underground natural gas storage facilities operated by Magyar Földgáztároló Zrt. (MFGT) are among the cornerstones of Hungary’s energy security. The largest of these facilities is located in Zsana, near Kiskunhalas in the southern part of Bács-Kiskun County.

Commissioned in 1996 and expanded and modernized several times since then, the facility has a storage capacity of 2.2 billion cubic meters. This volume represents more than two-thirds of Hungary’s total annual residential natural gas consumption.

Siemens compressors have long been used at the Zsana facility to inject natural gas arriving through transmission pipelines into underground storage formations, a process typically carried out during the summer months.

Electrical panels with controls bear “SIVACON” text; fluorescent lights and a smoke detector are set into a drop ceiling.

Siemens low-voltage switchgear at the Zsana facility. Source: MFGT

Cooling water ensures the continuous and safe operation of these compressors. Under normal operating conditions, the cooling water temperature must remain below 40°C. If this threshold is exceeded, overheating of the cooling systems and their cooling media can cause the equipment to shut down. Preventing such interruptions has become increasingly challenging in recent years due to prolonged periods of ambient temperatures exceeding 35°C.

To ensure operational continuity under changing temperature conditions, it became necessary to develop a cooling system with sufficient capacity to meet cooling requirements even during the most extreme summer heat.

The new installation's power supply was made possible by expanding the existing Siemens low-voltage power distribution switchgear with two additional panels, replacing the protective component in an existing spare panel, and installing new auxiliary power feeder units.

Siemens Zrt. supplied the equipment and components required for the project and also provided engineering support through its implementation partner, Univill-Trade Kft.

In addition to this latest upgrade, Siemens control technology is also used at the Zsana natural gas storage facility to manage gas injection and withdrawal operations.

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Kontaktai Spaudai

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com