Pranešimas Spaudai

Special solar power plant begins operation in Környe

2024 m. birželio 21 d.
Hungary

Hungary's first industrial solar power plant with automatically adjustable output based on real-time demand has been commissioned.

An increasing number of industrial companies in Hungary are taking significant steps to make their energy consumption more sustainable. However, integrating weather-dependent solar power plants into their systems cost-effectively can present challenges. Currently, industrial end users in Hungary are not permitted to feed surplus electricity generated by their solar power plants back into the public grid. As a result, these systems, which help reduce electricity consumption from the grid, must be equipped with reverse power protection (zero-export protection) and anti-islanding protection.

Intelligent control enables industrial companies to secure a predictable supply of green energy

Established technical solutions already exist for both types of protection in smaller power plants. For reverse power protection, data loggers are typically installed on inverters that convert direct current into alternating current, supplemented by an electricity meter. Anti-islanding protection generally relies on a dedicated protection device that monitors the presence of grid voltage and shuts down the power plant if the grid supply is lost due to a system fault. However, implementing similar solutions in larger power plants can be challenging. For example, numerous data loggers may be required, electricity consumption and generation may occur at different voltage levels, and the sheer size of the plant may mean that the points of measurement and intervention are several kilometers apart.

Siemens now offers an alternative to address these protection, control and monitoring challenges in large-scale power plants. Its new software-based solar power plant control solution combines substation data acquisition with advanced substation communication protocols.

This intelligent, automated system primarily addresses reverse power protection requirements through active control, managing even hundreds of inverters simultaneously. The communication network also serves as a means of implementing reverse power protection measures. The solution provides comprehensive plant-level monitoring by collecting information from power distribution equipment and inverters throughout the facility. It also transmits the necessary data from field-level devices to cloud-based aggregator monitoring systems, enabling remote monitoring of power generation and distribution across multiple power plants.

The system can also support facilities seeking to combine different renewable energy sources, such as integrating wind power generation. In addition to managing solar inverters and wind turbines, it can also control energy storage systems.

Until now, this type of control system designed to reduce electricity consumption from the grid had not been implemented in a large-scale industrial environment in Hungary.

A first in Hungary

The comprehensive control solution was first implemented at AGC Glass Hungary Kft.'s facility in Környe, which manufactures rear and side windows for the automotive industry. The solar power plant covers five hectares and consists of nearly 9,000 solar panels. With a DC capacity of 4.002 MWp and an annual electricity output of 4.8 GWh, the facility could generate enough electricity to meet the annual energy needs of approximately 1,900 households. The solar power plant was designed, built and operated by E.ON Energiatermelő Kft., which selected Siemens Zrt. as its technology partner during the planning phase to develop the control solution.

The plant's 34 inverters, each rated at 100 kVA and responsible for converting the direct current generated by the solar panels into alternating current, are monitored and controlled by Siemens' SICAM Photovoltaic Plant Control application, developed for the integration and intelligent automation of renewable energy sources. In addition to real-time control, the software provides power plant monitoring functions, tracking electricity generation using sensors that measure temperature, wind speed, humidity and solar irradiance.

Commissioned at the end of 2023, the system transmits the collected data to a cloud infrastructure operated by E.ON. This enables remote control of the solar park's electricity generation, as well as forecasting and scheduling of planned output. Since components supplied by third-party manufacturers have also been integrated into Siemens' control, data acquisition and monitoring system, the entire power plant can be managed as a single unit.

Towards microgrids

The project could also serve as a model for future microgrid installations in Hungary.

Microgrids are intelligent, local energy distribution systems that operate with a degree of independence from the public electricity grid, integrating connected electricity generation, consumption and storage equipment into a unified system. By transmitting real-time data from IoT-compatible low- and medium-voltage devices, they can also communicate with cloud-based platforms. These platforms can use artificial intelligence to optimize and automatically regulate energy management, continuously responding to changing conditions.

Microgrid technology has also helped make Siemens' headquarters in Vienna and Munich more sustainable.

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Kontaktai Spaudai

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com