Pranešimas Spaudai

These are the gifts going under the Christmas tree

2024 m. gruodžio 17 d.
Hungary

The Christmas gift-giving season presents challenges not only for us as shoppers but also for the toy industry. Dávid Gyaraki, Deputy Managing Director of REGIO JÁTÉK, Hungary’s leading toy retailer, explains how the company prepares for the year-end peak season, when it generates half of its annual revenue.

Christmas is a whole different planet – and filmstrips take on a new meaning

REGIO JÁTÉK’s operations undergo a complete transformation during November and December, requiring its logistics infrastructure to shift into overdrive. Black Friday has brought the biggest change in shopping habits in recent years, moving the start of the Christmas shopping season forward, although the frantic shopping rushes of previous years have become less intense.

LEGO and board games continue to dominate the bestseller lists, but surprisingly, the traditional filmstrip projector also consistently ranks among the most popular products.

In fact, it was Dávid Gyaraki’s father, who heads the company, who revived the filmstrip projector after the original model, previously manufactured by a record factory, became scarce on the market around 20 years ago.

The new version uses LED technology, does not overheat and is compatible with older filmstrips. Alongside classic Hungarian children’s stories such as Öreg néne őzikéje, new content is also being produced, including stories from the Bogyó és Babóca and Kufli series.

Board games aren't just for hardcore gamers

A visit to almost any toy store makes it clear that the board game market is experiencing a golden age. Alongside traditional competitive games, cooperative and association-based games are becoming increasingly popular, meaning that virtually everyone can find a type of game they enjoy.

Cooperative games focus on achieving shared goals, such as escaping from an island or saving the universe together, while association-based and abstract games encourage creativity.

Modern board games have also made the market more accessible. Today, it is not only hardcore gamers but also ordinary families who can enjoy meaningful shared experiences through board games.

There are also some unusual titles, such as the Scream board game, which incorporates technology into the experience. Through a mobile application, players may receive a phone call at a certain point in the game, and what they hear determines their next moves.

Interestingly, while mothers generally purchase most toys, fathers tend to take charge of choosing board games and are also happy to get involved in buying remote-controlled cars. After all, as REGIO JÁTÉK’s Deputy Managing Director puts it, “every toy brings joy to the child within us.”

Toys come from China, not the North Pole

The vast majority of toys originate from the Far East, primarily China, where a well-established industrial infrastructure enables large-scale manufacturing.

Hungarian production struggles to compete because of higher raw material costs and limited export channels. As a result, a finished product manufactured in China can sometimes cost less than the raw materials needed to produce it in Europe.

The toy industry also relies heavily on advance financing, meaning that, in theory, consumers could purchase all their Christmas presents as early as September.

At REGIO JÁTÉK, orders are placed at least six months in advance to ensure that toys arrive on time, by the end of August. The company's wholesale partners typically replenish their inventories in early September to supply retailers and customers.

Illustration - toys

Fast and accurate deliveries from an automated warehouse

Behind all this is an extensive logistics operation.

REGIO JÁTÉK’s 10,000-square-meter warehouse in Törökbálint, which has been operating since 2017, faces enormous demand during the peak season.

Goods arriving from China by sea are transported to Hungary by truck following EU customs clearance, before reaching the company’s central warehouse. There, products are sorted and stored or dispatched to the company’s 44 stores and online shop.

As sales volumes can increase four- or fivefold in the run-up to Christmas, stores may receive deliveries as often as twice a day during this period.

The warehouse was automated in 2020 to accelerate workflows, minimize errors and reduce excessive reliance on manual labor, as finding skilled employees is also a major challenge in warehouse operations.

The system, controlled and automated using Siemens technology, now places a box onto its 800-meter-long conveyor belt every 10 seconds, handling products ranging from the smallest filmstrips to two-meter-tall teddy bears.

In addition to improving efficiency, the investment has also increased inventory accuracy. The system sorts incoming goods based on barcodes, allowing it to determine, for example, how many units of a particular product should be stored and how many should be sent to stores.

The toy industry is becoming greener, too

Today, both the market and consumers increasingly expect toys to be manufactured more sustainably without compromising their appearance.

Initially, this conflicted with the traditional approach of Chinese suppliers, as implementing more sustainable production methods requires additional resources.

According to Dávid Gyaraki, parents primarily look for these solutions because of concerns about their children's health, although price sensitivity remains a decisive factor in purchasing decisions.

In the latest episode of the Voices of Industry podcast, Gyaraki also explains that the company’s commitment to environmentally conscious solutions extends beyond its finished products.

The operation of the Törökbálint warehouse is supported by solar collectors and an energy storage system, while the company has also had established practices for recycling toys and cardboard packaging for decades.

The full episode is available on the Siemens-világ podcast channel, as well as on the following platforms:

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Kontaktai Spaudai

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com