Persbericht

New SINAMICS S200 servo package is fit for future manufacturing applications

24 mei 2023

  • PROFINET and Pulse Train versions of single-axis AC/AC drive
  • Security chip and UMAC protection
  • Machine simulation is fit for digitalization
  • Global standards for worldwide use including UL, CE and SEMI 47
  • Built-in web-server and one-button tuning
  • For positioning, conveyorized moving and processing — whether standalone or operated by a motion controller

At AUTOMATE 2023, Siemens introduced its newest servo offering to the North American manufacturing industry. With the new SINAMICS S200 servo, comprising a SINAMICS S200 drive and SIMOTICS S-1FL2 motor with standard or flexible cable options, Siemens brings a new level of motion control to the stand-alone and networked machine market.

This new servo package expands the SINAMICS drive offering a variety of application possibilities to the standard servo market. The pulse train version allows a wide range of installed machines to easily integrate additional positioning axis using the onboard positioner. Meanwhile, a dynamic networking capability to motion control i.e., SIMATIC PLC expands its system capabilities in the PROFINET version. With a power range up to 7kW including low-, medium- and high-inertia offerings the 1FL2 permanent magnet motors with 17- or 21-bit encoders expand the performance, as well as scale to the widest range of standard servo requirements.

Easy setup is assured with the electronic type plate on the 1FL2 motor and one-button tunning in the S200 drive. The integrated brake resistor and integrated holding brake control add to the functions in the S200 servo-drive. High durability is designed in with the coated circuit boards (3C2) in the S200 and IP65 motors with metal connection solution. Built-in under-voltage protection is further provided.

For the engineering into a machine builder or machine user’s system, the embedded web-server or Startdrive software integrated into the Siemens TIA Portal is offered to fit user demand. Easy implementation of the SINAMICS S200 drive system on machines intended for global use is provided by universal standards and certification compliance.

SINAMICS S200 is included in the SINAMICS DriveSim Basic model and enables users to create a digital twin of the drive and PLC communication in the planning phase on a project to ensure proper sizing and operation of the equipment in use.

In the area of cybersecurity, the SINAMICS S200 for networked connection comes standard with integrated security, providing enhanced communication, integrity and authenticity checks to protect against tampered parameters, plus the drives offer User Management and Access Control (UMAC) within the TIA Portal.

Applications for the new SINAMICS S200 drive system range from the emerging battery market and other E-OEM segments to packaging, woodworking machinery, solar wafer production and many more.

The new SINAMICS S200 servo-drive system, comprising the S200 drive and SIMOTICS S-1FL2 servo motor with Motion Connect cabling, bring an enhanced level of performance to a stand-alone or networked machine for various market uses.

Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 75,000 employees internationally.

Siemens Corporation is a U.S. subsidiary of Siemens AG, a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power. In fiscal 2022, which ended on September 30, 2022, Siemens Group USA generated revenue of $18.6 billion and employs approximately 45,000 people serving customers in all 50 states and Puerto Rico.

Contactpersonen voor de pers

John Meyer
Phone: +1-847-952-4158
Email: john.meyer@siemens.com