Persbericht

Even these tiny details are state-of-the-art at the new MTK sports facility

19 mei 2025
Hungary

The MTK Sports Park on Kerepesi Road. Source: MTK

Siemens Zrt. supplied comfort automation components to the sports park on Kerepesi Road.

The new 25,000-square-meter MTK Sports Park on Kerepesi Road was built on a 94,000-square-meter site as a brownfield investment on the premises of the former Taurus rubber factory in Budapest. Completed by May 2025, the complex can accommodate 4,900 people and is suitable not only for hosting training sessions and competitions of club sports – such as basketball, handball, volleyball, rhythmic gymnastics, fencing, and football – including television broadcasts, but will also serve as a venue for exhibitions, conferences, concerts, and leisure events.

2 MTK Kerepesi úti sportpark - Forrás-MTK

The building of the MTK Sports Park on Kerepesi Road. Source: MTK

The energy management of the sports park, built in less than two years, is unique: water extracted from thermal wells 1,300 meters deep is used for the building’s heating and hot water systems, whose energy demand is covered by nearly one thousand solar panels with a total nominal capacity of 500 kWp.

For the details ensuring the circulation of this energy, the most advanced components currently available were also selected. Siemens Zrt., through its partner Épületautomatika Kft., supplied 31 intelligent valves to the air handling units and heating centers of the sports complex, as well as to the fan-coil systems responsible for heating the indoor courts.

These communication-capable valves, which are considered new even internationally, can connect to the building management systems controlling the rest of the building, allowing them to be remotely monitored and controlled through these systems or even via an independent cloud connection. Despite their complex functions, their installation and commissioning are particularly simple: with the help of a user-friendly smartphone application, even a mechanical installer without an IT background can configure their parameters.

The technology company also supplied an additional 29 butterfly valves and 46 motorized pressure-independent control valves (PICVs). These mechanical valves, equipped with an integrated differential pressure controller, automatically maintain the set flow rate regardless of pressure fluctuations occurring in the system, eliminating the need for additional balancing fittings. This means, for example, that they can automatically maintain the amount of water flowing through a pipe used for heating at a set level, regardless of how much the rest of the system requires at any given time.

3 Siemens Intelligens szelep - Forrás-Siemens

Siemens intelligent valve.

The world of sports facilities is not unfamiliar to Siemens Zrt.: its medium- and low-voltage power distribution solutions are used, for example, by the National Athletics Centre in Budapest, the Pick Arena in Szeged, and the Katalin Kovács National Kayak-Canoe Academy for youth development in Sukoró.

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Contactpersonen voor de pers

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com