Пресс-релиз

Ausgrid – first to go blue for the sake of green

29 ноября 2023 г.
Australia

Craig Wilson, Ausgrid, and Peter Halliday, Siemens, visit an Ausgrid site to see blue GIS in action.

Ausgrid, the largest distributor of electricity on Australia’s east coast, is the first organisation in Australia to install Siemens’ innovative blue gas insulated (GIS) medium voltage switchgear which uses climate-neutral 'clean air' in replacement of F-gas. 

Commonly used in industry, fluorinated greenhouse gases (F-gases) have high global warming potential. The SF6 (sulphur hexafluoride) variant that is traditionally used in insulation products has as much as 25,200 times the impact of CO2 on global warming. 

The use of blue GIS helps reduce Ausgrid’s carbon footprint and paves the way towards more sustainable, climate friendly grid infrastructure, supporting Australia’s pathway to net zero. As the electricity grid expands to cater for increased renewable energy, this grid expansion without F-gases will help stop Ausgrid’s carbon footprint from growing. 

“Ausgrid’s vision is for communities to have the power in a resilient, affordable and net zero future. Net zero is a strategic priority for us, and technological innovation will help us make a positive and sustainable impact on our electricity network that benefits our communities, the country and the planet. Installing new technology, such as Siemens’ blue GIS switchgear, is a significant milestone. This switchgear, instead of using the potent greenhouse gas SF6, uses completely carbon-neutral ambient air. Every step towards net zero is important, and the positive impact of the electricity industry moving away from damaging SF6 cannot be understated,” said Craig Wilson, Ausgrid Sustainability Manager.

"Every step towards net zero is important, and the positive impact of the electricity industry moving away from damaging SF6 cannot be understated," said Craig Wilson, Ausgrid Sustainability Manager.

Siemens’ blue GIS encompasses primary and secondary switchgear, with a maximum rated voltage of 24kV. Higher voltage ratings are under development. The overall footprint and dimensions of the blue GIS unit are identical to the SF6 versions which allows simple replacement.

Speaking on the announcement, Peter Halliday, CEO of Siemens Australia and New Zealand said, “The electricity grids in Australia play a pivotal role in the nation’s journey to net zero. The current and future challenges can only be met through innovative technology. It’s great to see Ausgrid be the first in Australia to install our blue GIS. Australia’s contribution to global carbon emissions is just over 1% and we need to embrace technologies that get us there faster and even helps the nation go beyond 1%.”

"The electricity grids in Australia play a pivotal role in the nation’s journey to net zero. The current and future challenges can only be met through innovative technology," said Peter Halliday, CEO, Siemens Australia & New Zealand.

The blue portfolio enables modernisation and expansion of existing power grids at the highest levels of safety and simultaneously reduces the ecological footprint without compromising on performance or economic feasibility.

According to the EU Commission, at EU level, F-gases currently account for 2.5% of total greenhouse gas emissions. In April 2022, the European Commission has released a legislative proposal to update the 2014 F-gas Regulation in order to more tightly control F-gases. Sulphur hexafluoride (SF6) is one of these gases. It has been used for more than 35 years in electricity transmission and distribution equipment as a switching and insulating gas. However, SF6 is the most potent greenhouse gas with an atmospheric residence of up to 3,200 years.

More information on GWP here: https://www.epa.gov/ghgemissions/understanding-global-warming-potentials

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare.

In fiscal 2023, which ended on September 30, 2023, the Siemens Group generated revenue of €77.8 billion and net income of €8.5 billion. As of September 30, 2023, the company employed around 320,000 people worldwide. Further information is available on the Internet at www.siemens.com.

Контакты пресс-службы

Krupa Uthappa

Phone: +61 427 601 578

Email: krupa.uthappa@siemens.com