The TIA Portal V20 comes with artificial intelligence capabilities.
The latest version of TIA Portal, V20, is entering the market with a significant expansion of features. Siemens’ engineering platform, used by industrial companies, supports engineers with capabilities such as artificial intelligence, integrated testing and cloud-based functionality. These enhancements can make tasks such as programming programmable logic controllers (PLCs) and human-machine interfaces (HMIs) even more efficient.
Advanced motion control and comprehensive compatibility
TIA Portal V20 has been designed to improve performance and simplify workflows, while also enabling users to take advantage of the latest automation capabilities.
Siemens has extended TIA Portal’s compatibility across its entire SIMATIC controller portfolio, meaning that version 20 supports the most advanced PLCs, including the new modular S7-1500 and the SIMATIC S7-1200 G2, which was unveiled at the Hannover Messe trade fair. These devices enable faster, more precise and safer manufacturing processes.
They also simplify complex machine-building tasks through integrated motion control functions, increased computing power and flexible machine safety solutions. The S7-1200 G2, for example, supports multi-axis control and the control of simple kinematic movements. Enhanced communication performance and increased memory capacity also ensure fast data processing.
The new Near Field Communication (NFC) functionality provides direct access to diagnostic, operational and device data, helping reduce machine downtime and enabling faster data handling.
In addition to improved PLC compatibility, TIA Portal V20 offers optimized programming capabilities and faster program execution analysis to support servicing and maintenance tasks.
Generative AI and cloud integration – with a focus on security
Generative artificial intelligence capabilities are also available in TIA Portal. Siemens Industrial Copilot simplifies programming tasks and accelerates troubleshooting.
The new version receives continuous functional and security updates, ensuring that users can always work with the latest technological solutions.
The platform also introduces innovations in cybersecurity and AI-assisted engineering. Among other features, it enables SIMATIC PLCs in production environments to be connected to a central user management system.
This access control functionality makes it easier for service technicians to access field devices using their corporate credentials. It also allows access rights for automation devices to be managed in a similar way to those within IT infrastructure.
The system enables seamless data exchange between TIA Portal, TIA Portal Cloud and Project Server Cloud, facilitating efficient collaboration across multiple work environments.
Automated cloud backups and continuous regression testing also help maintain high code quality.
The new version, scheduled for release in December, will be available to customers with a TIA Portal SUS (Software Update Service) subscription, who will automatically receive the upgrade license and installation files required to use it.