Reliability and sustainability take center stage.
Famous for the 4,478-meter-high Matterhorn, one of the tallest and most iconic peaks in the Alps, Zermatt is among Switzerland's most popular tourist destinations, recording approximately 2.5 million overnight stays in 2023.
The region is home to 38 mountain peaks exceeding 4,000 meters in elevation. Due to the town's remote location and challenging terrain, local communities face a unique set of difficulties. Extreme weather conditions, avalanches, significant elevation differences, thin air at high altitudes and steep slopes all make it difficult to develop reliable and sustainable infrastructure, highlighting the importance of innovative solutions.
Monte Rosa Hut
Located at an altitude of 2,883 meters, the modern, high-tech Monte Rosa Hut is one of Switzerland's most iconic mountain refuges. Reopened in 2010, the hut operates largely autonomously and is mostly self-sufficient in terms of energy supply.
Previously, the facility relied on 8.6 tons of lead-acid batteries for energy storage. By monitoring energy flows online, operators were able to assess the system's performance and decided to replace the batteries in 2021. Since then, 2.7 tons of lithium batteries have fulfilled the same function.
When the hut reopened, it was also equipped with Siemens building automation solutions. The comprehensive Desigo CC building management platform enables the centralized management of all building systems, including heating, ventilation and air conditioning (HVAC), shading, lighting, power supply, fire protection and security.
This allows operators to quickly review key equipment parameters, monitor critical areas and resolve potential issues.
In 2024, the system underwent another upgrade with the introduction of Siemens Building X, the company's latest building management platform. This scalable solution enables the digitalization of building operations, management and optimization, delivering improved performance and greater energy efficiency, ultimately making the hut's operation more sustainable.

Cable cars in the glacier paradise
Europe's highest cable car station is also located on the Matterhorn, at an altitude of 3,883 meters.
It forms part of an extensive network comprising 54 lift sections and 360 kilometers of cable car routes, offering breathtaking views of snow-covered peaks throughout the year. At lower elevations, visitors can also explore 400 kilometers of adventurous cycling and hiking trails during the summer months.
However, the mountainous terrain places particularly demanding requirements on infrastructure.
As a partner of Zermatt Bergbahnen AG, the company operating the cable car network, Siemens ensures a reliable low-voltage power supply and provides advanced control solutions.
These technologies enable transparent monitoring of the system and provide a comprehensive overview of energy management across the entire infrastructure, directly at the control units through a human-machine interface (HMI) or SCADA visualization system.
Thanks to standardized interfaces, subsystems and equipment from a wide range of manufacturers can be integrated into the control system, further simplifying operations for the cable car operator.