Comunicato stampa

Altair acquires Research in Flight, forging a new path for aerodynamic analysis

1 maggio 2024
Troy, Michigan, USA

  • Flagship solution, FlightStream®, pushes the boundaries of modern computational techniques

Altair, a global leader in computational intelligence, announced it has acquired Research in Flight, maker of FlightStream®, which provides computational fluid dynamics (CFD) software with a large footprint in the aerospace and defense sector and a growing presence in marine, energy, turbomachinery, and automotive applications.

FlightStream® is a user-friendly, yet powerful flow solver that bridges the gap between high-fidelity CFD simulations and the needs of engineers and designers. Its exceptionally fast computational speeds and low hardware footprint, coupled with a streamlined user interface and robust aerodynamic solver, make it an invaluable tool for early-stage rapid design iterations and in-depth aerodynamic studies for aerospace and defense applications and beyond. FlightStream® can capture subsonic to supersonic flows, including compressible effects and a unique surface vorticity capability. It leverages the strengths of panel method flow solvers and enhances them with modern computational techniques to provide a fast solver capable of handling complex aerodynamic phenomena.

“Our growth in the aerospace, defense, and surrounding industries has accelerated in recent years through our best-in-class computational intelligence solutions,” said James R. Scapa, founder and chief executive officer, Altair. “The integration of FlightStream® into our portfolio will enhance our offering with its specialized, modern, and efficient approach to meet the increasingly complex customer demands in these industries, including the urban air mobility and eVTOL sectors.”

FlightStream® allows for the rapid analysis of unconventional aircraft using a unique surface vorticity, flow-separation, and viscous analysis capability for both powered and unpowered configurations. It is augmented with integral boundary layer modeling, enabling users to capture viscous effects with a level of detail that is uncommon in traditional panel method applications. This integration facilitates a more comprehensive analysis of aerodynamic performance, providing insights that are crucial for design optimization.

“We are proud to be a standard tool in the aircraft designer’s toolbox,” said Vivek Ahuja, co-founder, Research in Flight. “Joining Altair will allow us to scale and reach countless engineers seeking best-in-class, powerful, and specialized tools for faster design iterations.”

In addition to Ahuja, Research in Flight was co-founded by Roy Hartfield who has dedicated more than 30 years to the study of aerodynamics, propulsion, statistical analysis of air vehicles, and aircraft research. Hartfield is an aerospace engineering professor at the Samuel Ginn College of Engineering at Auburn University.

FlightStream® is a United States Air Force network-approved software and is also used at NASA Ames and Langley Research Centers, as well as by the U.S. Army. It will be integrated into the Altair® HyperWorks® design and simulation platform and be available via Altair Units.

Altair is a global leader in computational intelligence that provides software and cloud solutions in simulation, high-performance computing (HPC), data analytics, and AI. Altair is part of Siemens Digital Industries Software. To learn more, please visit altair.com or sw.siemens.com.

Contatti per la stampa

Zulmira Almeida

Tel: (+33) 06 77 19 80 52; E-mail: marie.almeida@siemens.com

Anna Romanelli - ITALMARCO

Tel: (+39) 02 70 10 46 45 – (+39) 347 745 04 09; E-mail: anna@italmarco.com