Comunicato stampa

Siemens’ new Calibre DesignEnhancer boosts Samsung Foundry design quality and speeds time to market

7 dicembre 2023
Plano, Texas, USA

Siemens announces availability of a new process design kit (PDK) from Samsung Foundry that helps mutual customers boost the reliability, quality and robustness of their next-generation integrated circuit (IC) designs manufactured using the foundry’s latest processes.

Siemens Digital Industries Software today announces availability of a new process design kit (PDK) from Samsung Foundry that helps mutual customers boost the reliability, quality and robustness of their next-generation integrated circuit (IC) designs manufactured using the foundry’s latest processes. The design kit supports Siemens’ Calibre® DesignEnhancer software solution, which is the latest addition to the company’s EDA industry-leading Calibre® nmPlatform for IC verification. 

Unveiled in July at the 2023 Design Automation Conference, the Calibre DesignEnhancer solution provides multiple use models that perform automatic layout optimizations to improve power robustness and reduce design cycles during design implementation. Calibre DesignEnhancer works with the Samsung PDK to help mutual customers achieve substantial first-pass gains in designer productivity when compared to traditional place-and-route (P&R) processes, which often require design teams to conduct multiple runs to achieve the same Calibre nmDRC-correct results.

“Samsung Foundry has a long and successful track record of leveraging Siemens’ Calibre software to provide our mutual customers with ‘Calibre nmDRC-correct’ designs. Based on the results we have seen, the Calibre DesignEnhancer solution provides our mutual customers a step function increase in via insertion efficiency, and faster turnaround time compared to classic approaches to the problem,” said JoongWon Jeon, Distinguished Engineer of Foundry Technology Development Team at Samsung Electronics.

The Calibre DesignEnhancer via insertion use model automatically inserts additional Calibre nmDRC-correct vias into layouts to reduce resistance that can minimize both voltage (IR) drop and electrostatic discharge (ESD) events in IC designs. The Calibre DesignEnhancer via optimization use model can add up to millions more vias than previously possible.

“The incorporation of the Calibre DesignEnhancer solution with Samsung Foundry’s most advanced processes demonstrates what can be possible when world-class IC EDA and fabrication players partner to help mutual customers successfully and efficiently fabricate new devices in leading-edge technologies,” said Michael White, senior director, Physical Verification Product Management, Siemens Digital Industries Software.

Siemens Digital Industries Software aiuta le organizzazioni di tutte le dimensioni ad affrontare la digital transformation utilizzando il software, l’hardware ed i servizi della piattaforma di business Siemens Xcelerator. Il software offerto da Siemens, unitamente alle tecnologie per la realizzazione di completi digital twin, consentono alle aziende di ottimizzare i propri processi di progettazione, di ingegnerizzazione e di produzione, per trasformare le idee di oggi in prodotti sostenibili del futuro. Da singoli chip fino a interi sistemi, dai prodotti ai processi, in tutti i settori. Siemens Digital Industries Software– Accelerating transformation.

Nota: un elenco dei marchi rilevanti di proprietà di Siemens è consultabile qui. Tutti gli altri marchi menzionati appartengono ai rispettivi proprietari.

Contatti per la stampa

Zulmira Almeida

Tel: (+33) 06 77 19 80 52; E-mail: marie.almeida@siemens.com

Anna Romanelli - ITALMARCO

Tel: (+39) 02 70 10 46 45 – (+39) 347 745 04 09; E-mail: anna@italmarco.com