보도 자료

Siemens transforms computational lithography for next-generation AI semiconductors with NVIDIA cuLitho

2026년 10월 14일
Plano, Texas, USA

  • Collaboration between Siemens and NVIDIA delivers up to 12x acceleration for full-chip optical proximity correction (OPC) workloads in lithography 
  • Enables practical full-chip optimization of photomasks for High Numerical Aperture Extreme Ultraviolet EUV lithography (High-NA EUV) lithography using the most advanced computational lithographic methods, including inverse lithography technology (ILT) 
  • Addresses the critical runtime and complexity challenges of leading-edge patterning for AI compute and memory devices

Siemens today announced significant advances in its collaboration with NVIDIA to accelerate computational lithography workflows. By integrating NVIDIA cuLitho, a CUDA-X library for GPU-accelerated computational lithography, with Calibre® manufacturing software, Siemens is enabling semiconductor manufacturers to overcome the runtime-limited challenges of advanced patterning, making next-generation AI semiconductors a manufacturing reality.

The patterning bottleneck challenge

As the industry aggressively moves toward leading-edge process nodes, the complexity of lithographic patterning has increased exponentially. Traditional optical proximity correction (OPC) and computational lithography techniques face a "runtime wall." The transition to High-NA EUV and the requirement for advanced curvilinear patterning - such as Inverse Lithography Technology (ILT) - demand massive computational resources.

Without acceleration, these essential techniques are often too slow for full-chip, manufacturing-scale deployment, and forcing engineering teams to make trade-offs between optimization depth and project schedules. This creates a risk of lithographic hotspots and reduced process margins, which can impact yield for the most advanced AI compute and memory devices.

GPU-accelerated patterning to radically accelerate lithography simulation

Siemens and NVIDIA are transforming this challenge into an enabling technology. By delivering at least 10x acceleration for key lithography simulation workloads, the collaboration allows manufacturers to perform more comprehensive optimization and identify potential hotspots before tapeout.

“Computational lithography has traditionally been one of the most compute-intensive stages of the design-to-manufacturing flow,” said Ankur Gupta, executive vice president, EDA IC Portfolio, Siemens. “By combining Siemens’ signoff-grade Calibre technology with NVIDIA’s GPU acceleration, we are giving our customers the ability to deploy advanced patterning strategies like curvilinear ILT at scale. This isn't just about speed; it's about enabling the precision required for the next generation of AI infrastructure.”

“Next-generation chips are pushing the limits of manufacturing complexity, making computational lithography more critical than ever,” said Tim Costa, vice president and general manager of industrial and computational engineering at NVIDIA. “By bringing NVIDIA cuLitho acceleration to Siemens’ Calibre, we’re enabling engineers to tackle increasingly intricate patterns and explore more extensive optimizations needed to manufacture the world’s most advanced chips.”

Measurable value to chip and photomask manufacturers

The collaboration provides semiconductor and mask manufacturers with measurable performance gains across critical computational lithography workflows. Verified engineering data supports simulation speed-ups ranging from at least 10x to 17x for key workloads, helping make full-chip curvilinear patterning practical for High-NA EUV production.

By reducing simulation runtimes, manufacturers can complete more iterations in less time, identify lithographic hotspots earlier and improve process margins before tapeout. This faster turnaround can also help accelerate manufacturing readiness and support the deployment of new AI silicon.

To learn more about Siemens’ advanced semiconductor design and manufacturing solutions, please visit: https://blogs.sw.siemens.com/calibre/2026/10/14/the-virtuous-cycle-of-silicon-how-siemens-is-accelerating-the-era-of-physical-ai-with-nvidia-culitho/

지멘스 디지털 인더스트리 소프트웨어 소개

지멘스 디지털 인더스트리 소프트웨어는 규모에 상관없이 모든 기업들이 Siemens Xcelerator 비즈니스 플랫폼의 소프트웨어, 하드웨어, 서비스를 사용해 디지털 전환을 추진하도록 지원한다. 지멘스의 소프트웨어와 포괄적인 디지털 트윈을 통해 기업은 설계, 엔지니어링, 제조 프로세스를 최적화함으로써 오늘의 아이디어를 미래의 지속가능한 제품으로 만들어낼 수 있다. 칩부터 전체 시스템까지, 제품부터 프로세스까지, 모든 산업을 아우른다.Siemens Digital Industries Software – Accelerating transformation.

지멘스 디지털 인더스트리 소개

지멘스 디지털 인더스트리(DI)는 공정과 개별 제조 산업에 속한 모든 규모의 기업이 전체 가치사슬에서 디지털·지속가능성 전환을 가속화할 수 있도록 지원한다. 지멘스의 최첨단 자동화와 소프트웨어 포트폴리오는 제품과 생산의 설계, 구현, 최적화를 혁신적으로 개선한다. 개방형 디지털 비즈니스 플랫폼인 Siemens Xcelerator를 통해 보다 쉽고 빠르며 확장 가능한 프로세스를 구현할 수 있다. DI는 파트너·생태계와 함께 고객이 지속 가능한 디지털 기업이 될 수 있도록 지원한다. 전 세계적으로 약 7만여 명의 직원들이 DI에 근무하고 있다.

지멘스 소개

독일 베를린과 뮌헨에 본사를 둔 지멘스는 산업, 인프라, 모빌리티, 헬스케어 등의 분야에 역량을 집중하고 있는 세계적인 기술 기업이다. 지멘스는 모든 사람을 위해 일상을 변화시키는 기술을 개발하는 것을 목적으로 한다. 지멘스는 현실과 디지털 세계를 결합함으로써 고객이 디지털과 지속 가능성 전환을 가속화해 보다 효율적인 공장, 살기 좋은 도시, 지속 가능한 운송을 구현할 수 있도록 지원한다. 산업용 AI 분야의 선두주자인 지멘스는 심층적인 분야 전문성을 바탕으로 생성형 AI를 포함한 AI 기술을 실제 응용 분야에 적용해 다양한 산업의 고객이 AI를 접근 가능하고 효과적으로 활용할 수 있도록 한다. 또한 지멘스는 헬스케어 분야의 혁신을 선도하는 세계적 의료기술 기업이자 상장 계열사인 지멘스 헬시니어스의 최대 지분을 보유하고 있다. 지멘스는 모두를 위한 모든 곳에서의 지속 가능한 솔루션을 제공한다.

2025년 9월 30일 종료된 2025 회계연도에 지멘스 그룹의 매출액은 789억 유로, 순이익은 104억 유로다. 2025년 9월 30일 기준 전 세계적으로 31만 8천 명의 직원이 근무하고 있다. 자세한 내용은 https://www.siemens.com/에서 확인할 수 있다.

지멘스 관련 상표 목록은 여기에서 찾아볼 수 있다. 기타 상표는 해당 소유자에게 속한다.

언론 연락처