보도 자료

Haddy scales AI-enabled adaptative microfactories with Siemens Xcelerator

2026년 6월 1일
Plano, Texas, USA

Haddy has adopted the Siemens Xcelerator open digital business platform, to scale local additive manufacturing using circular materials across industries including furniture, marine and defense (Image credit: Haddy)
  • Additive manufacturing innovator scales local production while keeping materials in use through a circular additive manufacturing model
  • Design and manufacturing digital thread helps Haddy produce large-format parts consistently across microfactories
  • Software-defined manufacturing supports repeatable robotic additive production as Haddy expands its distributed model

Siemens today announced that Haddy, a U.S.-based additive manufacturing company, has adopted the Siemens Xcelerator open digital business platform, to scale local additive manufacturing using circular materials across industries including furniture, marine and defense. 
 
Founded around the idea that additive manufacturing can support both local production and circular material use, Haddy produces large-format components using robotic additive manufacturing processes and recyclable and biodegradable materials designed to stay in use. Products are made to be taken back at end of life, reprocessed into feedstock and returned to production, helping to reduce waste and keep materials out of landfill. Materials are sourced domestically in the U.S. to help reduce transportation-related emissions while supporting local supply chains.

“Our goal is to keep materials in use and production close to where products are needed,” said Jay Rogers, chief executive officer, Haddy. “Adopting Siemens Xcelerator helps us connect design, automation and manufacturing in a way that supports circularity, local sourcing and rapid iteration while using data and AI to continuously improve how our microfactories operate.”

siemens-haddy-newsroom-02-1280x720

Haddy has adopted the Siemens Xcelerator open digital business platform, to scale local additive manufacturing using circular materials across industries including furniture, marine and defense (Image credit: Haddy)

Haddy delivers this model through a network of digitally standardized, AI-enabled microfactories. By producing closer to where products are needed and relying on data and software to maintain consistency across sites, the company aims to reduce supply-chain complexity while supporting more resilient, low-waste production.  
 
To support this approach, Haddy uses Siemens Xcelerator to connect product design, manufacturing planning and automation through a consistent digital thread. Siemens’ Designcenter™ software is used to design large-format parts produced through additive manufacturing and prepare those designs for robotic production. Teamcenter® software manages product data and configuration across sites, while SINUMERIK, Siemens’ CNC control platform primarily for machine tools, is used to provide high-precision motion control and execution on the shop floor, including the integration of industrial robots. In Haddy’s microfactories, SINUMERIK orchestrates robotic additive manufacturing systems, combining CNC-based path control with industrial robot kinematics, including CEAD’s large-format robotic extrusion platforms.  

siemens-haddy-newsroom-03-1280x720

Haddy uses Siemens Xcelerator to connect product design, manufacturing planning and automation through a consistent digital thread
 
As part of this adoption, Haddy is expanding its use of Siemens’ software, as the company scales its distributed production model. It has adopted Simcenter™ Optistruct® software to assist with product optimization and validation of its large-scale products. Alongside this, Haddy is leveraging NX™ X Manufacturing, a cloud‑enabled manufacturing solution, to define build strategies, support NC programming, simulation and execution of complex large‑format robotic additive manufacturing processes. Haddy also uses of subtractive CNC machining as part of its production process using the same toolset providing advanced computer aided machining (CAM) part programming, simulation and verification capabilities.

NX X Manufacturing allows Haddy to produce parts from the size of a shoe box to an entire boat with precision and quality, while inherent cloud accessibility means Haddy can meet the needs of its rapidly expanding business with low IT overhead while using value-based licensing tokens to expand production with additional software capabilities.

siemens-haddy-newsroom-04-1280x720

Haddy is expanding its use of Siemens’ software, as the company scales its distributed production model.

“Haddy is showing how manufacturers can rethink production by combining the power of the AI-enabled digital twin and local manufacturing with circular material strategies,” said Tony Hemmelgarn, president and CEO, Siemens Digital Industries Software. “By building a digitally connected, software‑defined manufacturing model, Haddy is creating a scalable approach that helps maintain consistency across sites while supporting more resilient and sustainable production. This same approach can help other manufacturers adapt faster, reduce waste and bring production closer to where products are needed.”

Haddy will also share its perspective on scaling large‑format additive manufacturing and digitally enabled microfactories at Realize LIVE Americas today in Detroit, where Jay Rogers, CEO, Haddy, is delivering a keynote focused on the future of sustainable, AI‑enabled manufacturing.

To learn more about how Siemens Xcelerator helps innovators and pioneers to build the future, visit https://www.siemens.com/en-us/company/digital-transformation/

지멘스 디지털 인더스트리 소프트웨어 소개

지멘스 디지털 인더스트리 소프트웨어는 규모에 상관없이 모든 기업들이 Siemens Xcelerator 비즈니스 플랫폼의 소프트웨어, 하드웨어, 서비스를 사용해 디지털 전환을 추진하도록 지원한다. 지멘스의 소프트웨어와 포괄적인 디지털 트윈을 통해 기업은 설계, 엔지니어링, 제조 프로세스를 최적화함으로써 오늘의 아이디어를 미래의 지속가능한 제품으로 만들어낼 수 있다. 칩부터 전체 시스템까지, 제품부터 프로세스까지, 모든 산업을 아우른다.Siemens Digital Industries Software – Accelerating transformation.

지멘스 디지털 인더스트리 소개

지멘스 디지털 인더스트리(DI)는 공정과 개별 제조 산업에 속한 모든 규모의 기업이 전체 가치사슬에서 디지털·지속가능성 전환을 가속화할 수 있도록 지원한다. 지멘스의 최첨단 자동화와 소프트웨어 포트폴리오는 제품과 생산의 설계, 구현, 최적화를 혁신적으로 개선한다. 개방형 디지털 비즈니스 플랫폼인 Siemens Xcelerator를 통해 보다 쉽고 빠르며 확장 가능한 프로세스를 구현할 수 있다. DI는 파트너·생태계와 함께 고객이 지속 가능한 디지털 기업이 될 수 있도록 지원한다. 전 세계적으로 약 7만여 명의 직원들이 DI에 근무하고 있다.

지멘스 소개

독일 베를린과 뮌헨에 본사를 둔 지멘스는 산업, 인프라, 모빌리티, 헬스케어 등의 분야에 역량을 집중하고 있는 세계적인 기술 기업이다. 지멘스는 모든 사람을 위해 일상을 변화시키는 기술을 개발하는 것을 목적으로 한다. 지멘스는 현실과 디지털 세계를 결합함으로써 고객이 디지털과 지속 가능성 전환을 가속화해 보다 효율적인 공장, 살기 좋은 도시, 지속 가능한 운송을 구현할 수 있도록 지원한다. 산업용 AI 분야의 선두주자인 지멘스는 심층적인 분야 전문성을 바탕으로 생성형 AI를 포함한 AI 기술을 실제 응용 분야에 적용해 다양한 산업의 고객이 AI를 접근 가능하고 효과적으로 활용할 수 있도록 한다. 또한 지멘스는 헬스케어 분야의 혁신을 선도하는 세계적 의료기술 기업이자 상장 계열사인 지멘스 헬시니어스의 최대 지분을 보유하고 있다. 지멘스는 모두를 위한 모든 곳에서의 지속 가능한 솔루션을 제공한다.

2025년 9월 30일 종료된 2025 회계연도에 지멘스 그룹의 매출액은 789억 유로, 순이익은 104억 유로다. 2025년 9월 30일 기준 전 세계적으로 31만 8천 명의 직원이 근무하고 있다. 자세한 내용은 https://www.siemens.com/에서 확인할 수 있다.

언론 연락처