보도 자료

Siemens powers the next phase of industrial AI with Intelligence Center X

2026년 6월 1일
Realize LIVE Americas, Detroit, Michigan, USA

  • Embeds AI agents alongside people to scale industrial AI into a hybrid workforce at production level, enabling organizations to move beyond pilots and operate with speed, control and consistency
  • Connects industrial data, workflows and AI agents in one governed system, unifying enterprise data and lifecycle context, empowering teams to collaborate with AI in context-rich, human-in-the-loop processes across the business
  • Delivers measurable operational impact at scale by reducing manual effort, accelerating issue resolution and improving decision-making with results proven in real-world deployments
  • Customers are already delivering measurable results including a 95 percent reduction in manual effort and 85 percent faster production issue resolution
  • Siemens Intelligence Center X, part of Siemens Xcelerator, helps customers scale digital transformation with production-ready industrial AI

Siemens today announced Intelligence Center X, new industrial AI orchestration software designed to help organizations turn industrial AI from isolated experimentation into scalable, real world business impact through a hybrid workforce where people and AI agents work together with shared context, workflows and lifecycle intelligence.

By connecting data, models and workflows on a single governed foundation, Intelligence Center X enables companies to deploy AI-driven applications and agents faster, with full traceability and control. Intelligence Center X combines the Mendix™ low-code platform with Siemens’ Graph Studio and AI Studio software from the Rapidminer® portfolio to create the enterprise context, business-specific lifecycle intelligence, and orchestrated agents and intelligent applications businesses needed to turn AI ambition into real value gains. Across industries, companies have invested in AI but are struggling to scale beyond pilots because data is fragmented, governance is inconsistent, and AI insight does not connect to real workflows. Intelligence Center X is designed to close that gap as the production-ready system that orchestrates people and AI agents together, on top of what enterprises already own, with full auditability and policy controls.

“Intelligence Center X helps organizations move beyond AI experimentation by embedding intelligence directly into everyday workflows, where it can be governed, scaled and trusted. When AI is connected to real business processes and enterprise data, it delivers measurable impact at scale,” said Tony Hemmelgarn, president and CEO, Siemens Digital Industries Software. “AI only delivers real value when it is embedded in how work gets done. Intelligence Center X brings together enterprise data with industrial ontologies and Siemens’ knowledge graph capabilities in a governed environment to empower organizations to apply AI with confidence and achieve consistent, measurable outcomes.”

Customers already delivering measurable outcomes

Vivix Vidros Planos, Brazil’s leading flat glass manufacturer, deployed a portfolio of nearly 30 Mendix applications connecting OT and IT data across SAP S/4HANA, Siemens Industrial Edge, and Snowflake. Results include an 85 percent reduction in production issue resolution time, 6,000 hours of manual work recaptured in a single year, and customer complaint resolution compressed from five days to under one. Vivix’s AI-powered Virtual Engineer, built on Intelligence Center X with Amazon Bedrock and Claude from Anthropic, is now advancing toward a full digital twin strategy using the multi-agent capabilities in Intelligence Center X.

“With this system, we are ready for the agentic future, enabling our people and AI to work together in a more connected and productive way,” said Aristóteles Terceiro Neto, industrial transformation manager, Vivix Vidros Planos. “We are already seeing significant enterprise value, including up to 4x faster resolution times in quality-related investigations, as well as measurable improvements in how we support decision-making on the shop floor.”

"Axiz is among the first enterprises globally to deploy Intelligence Center X as a full agentic enterprise system. Integrating the AI/ML modeling capabilities, application development and process orchestration for an end-to-end pricing use case, Axiz achieved a 95 percent reduction in manual effort and 100 percent accuracy in data ingestion,” said Andrew Moodley, chief cloud, digital and marketing officer, Axiz. “Axiz is the first customer globally to integrate Intelligence Center X for our pricing use case. AI/ML development acts as the brain, while the application development and orchestration capabilities act as the body.”

Building the data foundation for agentic execution

Intelligence Center X is designed to connect industrial data across engineering, manufacturing, supply chain and service into shared lifecycle intelligence that AI can act on. As part of the Siemens Xcelerator portfolio, Intelligence Center X is designed to work alongside existing enterprise and operational data solutions to enable agentic workflows to operate with trusted data across the broader ecosystem. This approach is supported by Siemens’ data and cloud ecosystem partners.

“We are genuinely excited about the new capabilities Intelligence Center X brings to Snowflake customers," said Amy Kodl, senior vice president, Worldwide Alliances and Channels, Snowflake. "It works with their existing Snowflake data, complements capabilities like Snowflake Semantic Views and Cortex AI and shares our relentless focus on being easy, connected and trusted.”

Three deployment models

Intelligence Center X deploys in three patterns: layered on Siemens AI products to amplify lifecycle intelligence with out-of-the-box industrial ontologies; as a standalone platform for asset-intensive organizations running other OT vendors; or as a pure agentic enterprise platform for financial services, insurance, healthcare, government, and retail organizations that need production-grade AI execution with full auditability.

Availability

To learn more about Intelligence Center X, visit https://www.mendix.com/whats-new/

지멘스 디지털 인더스트리 소프트웨어 소개

지멘스 디지털 인더스트리 소프트웨어는 규모에 상관없이 모든 기업들이 Siemens Xcelerator 비즈니스 플랫폼의 소프트웨어, 하드웨어, 서비스를 사용해 디지털 전환을 추진하도록 지원한다. 지멘스의 소프트웨어와 포괄적인 디지털 트윈을 통해 기업은 설계, 엔지니어링, 제조 프로세스를 최적화함으로써 오늘의 아이디어를 미래의 지속가능한 제품으로 만들어낼 수 있다. 칩부터 전체 시스템까지, 제품부터 프로세스까지, 모든 산업을 아우른다.Siemens Digital Industries Software – Accelerating transformation.

지멘스 디지털 인더스트리 소개

지멘스 디지털 인더스트리(DI)는 공정과 개별 제조 산업에 속한 모든 규모의 기업이 전체 가치사슬에서 디지털·지속가능성 전환을 가속화할 수 있도록 지원한다. 지멘스의 최첨단 자동화와 소프트웨어 포트폴리오는 제품과 생산의 설계, 구현, 최적화를 혁신적으로 개선한다. 개방형 디지털 비즈니스 플랫폼인 Siemens Xcelerator를 통해 보다 쉽고 빠르며 확장 가능한 프로세스를 구현할 수 있다. DI는 파트너·생태계와 함께 고객이 지속 가능한 디지털 기업이 될 수 있도록 지원한다. 전 세계적으로 약 7만여 명의 직원들이 DI에 근무하고 있다.

지멘스 소개

독일 베를린과 뮌헨에 본사를 둔 지멘스는 산업, 인프라, 모빌리티, 헬스케어 등의 분야에 역량을 집중하고 있는 세계적인 기술 기업이다. 지멘스는 모든 사람을 위해 일상을 변화시키는 기술을 개발하는 것을 목적으로 한다. 지멘스는 현실과 디지털 세계를 결합함으로써 고객이 디지털과 지속 가능성 전환을 가속화해 보다 효율적인 공장, 살기 좋은 도시, 지속 가능한 운송을 구현할 수 있도록 지원한다. 산업용 AI 분야의 선두주자인 지멘스는 심층적인 분야 전문성을 바탕으로 생성형 AI를 포함한 AI 기술을 실제 응용 분야에 적용해 다양한 산업의 고객이 AI를 접근 가능하고 효과적으로 활용할 수 있도록 한다. 또한 지멘스는 헬스케어 분야의 혁신을 선도하는 세계적 의료기술 기업이자 상장 계열사인 지멘스 헬시니어스의 최대 지분을 보유하고 있다. 지멘스는 모두를 위한 모든 곳에서의 지속 가능한 솔루션을 제공한다.

2025년 9월 30일 종료된 2025 회계연도에 지멘스 그룹의 매출액은 789억 유로, 순이익은 104억 유로다. 2025년 9월 30일 기준 전 세계적으로 31만 8천 명의 직원이 근무하고 있다. 자세한 내용은 https://www.siemens.com/에서 확인할 수 있다.

지멘스 관련 상표 목록은 여기에서 찾아볼 수 있다. 기타 상표는 해당 소유자에게 속한다.

언론 연락처