보도 자료

Siemens and NVIDIA advance AI-powered PCB inspection from Digital Twin to factory

2026년 10월 21일
Plano, Texas, USA

  • Siemens and NVIDIA collaborate to boost engineering productivity, increase quality and bring automated optical inspection preparation into the virtual world 
  • Virtual golden board representations and synthetic data support inspection preparation before the first physical printed circuit board (PCB) reaches the production line 
  • Project targets include up to 85 percent less manual engineering effort, more than 40 percent fewer false calls and more than 5 percent first-pass yield improvement

Siemens today announced a new collaboration with NVIDIA to develop adaptive AI-powered manufacturing capabilities that combine industrial software, Siemens’ Digital Twin technology and NVIDIA Cosmos to accelerate production planning, inspection preparation and optimization.

The collaboration combines Siemens’ Teamcenter® software for product lifecycle management (PLM) and Process Preparation X with NVIDIA Cosmos to create a new AI-powered workflow for PCB inspection, helping electronics manufacturers prepare and optimize automated optical inspection (AOI) processes before physical production begins.

The solution is being demonstrated at Siemens Electronics Factory Erlangen, Siemens' Customer Zero for adaptive AI-powered production – with the goal of creating a highly adaptive factory that can rapidly introduce near daily changes (3 to 5 times a week) without disruption. 

siemens nvidia pcba digital twin factory 02

Digital twin of SMT AOI inspection area at Siemens Electronics Factory Erlangen created using the Digital Twin Composer

“By connecting the comprehensive Digital Twin to the shop floor and AI we are improving both line productivity and product quality. At the Erlangen factory, we're demonstrating how the deterministic nature of Siemens’ Digital Twin is the foundation for leveraging physics AI for preparing production,” said Mark Hindsbo, executive vice president operations software, Siemens. “By leveraging a ‘virtual’ golden board, electronics manufacturers can change production dramatically quicker without taking the line out of production. This enables electronics manufacturers to respond more quickly to change and helps reach production readiness at scale and speed – while helping to reduce manual engineering effort, accelerate AOI readiness and improve manufacturing quality.”  

“Manufacturers shouldn’t have to wait for the first physical circuit board to start preparing inspection,” said Rev Lebaredian, vice president, Physical AI Simulation at NVIDIA. “By combining Siemens’ industrial software and manufacturing expertise with NVIDIA Cosmos, we can generate synthetic images of good and defective boards to prepare inspection virtually—helping manufacturers bring new products into production faster.” 

Traditionally, introducing a new product or product variant requires a physical prototype before optical inspection processes can be prepared and trained for quality control. The new approach moves more of that work into the virtual world. Teamcenter provides PCB design, bill of materials and component information while Process Preparation X validates, normalizes and assembles this information into a Digital Twin of the printed circuit board assembly (PCBA). This provides the comprehensive product and manufacturing context needed to prepare inspection before the first physical board reaches the production line. 

This Digital Twin of the “perfect” reference board, often referred to as the “golden board,” is used with NVIDIA Cosmos to create a fully photorealistic virtual golden board along with synthetic photorealistic samples that represent both good and false conditions created during production.  Siemens uses NVIDIA Cosmos Data Factory to generate synthetic circuit-board defect images, enabling inspection-machine calibration before physical boards are produced.

The workflow then extends into production through an AI-supported secondary inspection capability. When an AOI system identifies a potential defect, the secondary inspection capability can help analyze the detected condition and determine whether it represents a real defect or a false call. Together, these technologies are intended to create an end-to-end digital and AI-supported workflow spanning virtual AOI preparation, calibration and inspection support once production begins. 

siemens nvidia pcba digital twin factory 07

Images of the Golden Board and potential defects are automatically produced from the digital twin of the PCB using Process Preparation X software and NVIDIA Cosmos

Customer Zero at Siemens Electronics Factory, Erlangen 

The collaboration is being demonstrated at the Siemens Electronics Factory in Erlangen, Germany, which serves as Customer Zero for broader Siemens and NVIDIA work on adaptive, autonomous and AI-powered production. The factory contributes the manufacturing use case, production environment and subject-matter expertise in a highly adaptable, high-mix environment with ever-changing production processes. The project is targeting up to 85 percent less manual engineering effort in AOI program generation – with 40 percent fewer false calls and more than 5 percent first-pass yield improvement.  

For manufacturers, the intended value is earlier inspection preparation, reduced manual engineering effort, lower dependency on physical samples, better-calibrated inspection processes, reduced manual verification, faster production readiness and improved manufacturing quality. The collaboration also demonstrates how the Digital Twin and industrial AI can connect engineering intent with real-world inspection across the digital and real stages of production and how the comprehensive Digital Twin evolves from a virtual representation of the product into an active foundation for AI-powered manufacturing and quality processes. 

To learn more about how Siemens is exploring the future of physical AI with Process Preparation X, visit https://www.siemens.com/en-us/products/tecnomatix/process-preparation-software/ 

지멘스 디지털 인더스트리 소프트웨어 소개

지멘스 디지털 인더스트리 소프트웨어는 규모에 상관없이 모든 기업들이 Siemens Xcelerator 비즈니스 플랫폼의 소프트웨어, 하드웨어, 서비스를 사용해 디지털 전환을 추진하도록 지원한다. 지멘스의 소프트웨어와 포괄적인 디지털 트윈을 통해 기업은 설계, 엔지니어링, 제조 프로세스를 최적화함으로써 오늘의 아이디어를 미래의 지속가능한 제품으로 만들어낼 수 있다. 칩부터 전체 시스템까지, 제품부터 프로세스까지, 모든 산업을 아우른다.Siemens Digital Industries Software – Accelerating transformation.

지멘스 디지털 인더스트리 소개

지멘스 디지털 인더스트리(DI)는 공정과 개별 제조 산업에 속한 모든 규모의 기업이 전체 가치사슬에서 디지털·지속가능성 전환을 가속화할 수 있도록 지원한다. 지멘스의 최첨단 자동화와 소프트웨어 포트폴리오는 제품과 생산의 설계, 구현, 최적화를 혁신적으로 개선한다. 개방형 디지털 비즈니스 플랫폼인 Siemens Xcelerator를 통해 보다 쉽고 빠르며 확장 가능한 프로세스를 구현할 수 있다. DI는 파트너·생태계와 함께 고객이 지속 가능한 디지털 기업이 될 수 있도록 지원한다. 전 세계적으로 약 7만여 명의 직원들이 DI에 근무하고 있다.

지멘스 소개

독일 베를린과 뮌헨에 본사를 둔 지멘스는 산업, 인프라, 모빌리티, 헬스케어 등의 분야에 역량을 집중하고 있는 세계적인 기술 기업이다. 지멘스는 모든 사람을 위해 일상을 변화시키는 기술을 개발하는 것을 목적으로 한다. 지멘스는 현실과 디지털 세계를 결합함으로써 고객이 디지털과 지속 가능성 전환을 가속화해 보다 효율적인 공장, 살기 좋은 도시, 지속 가능한 운송을 구현할 수 있도록 지원한다. 산업용 AI 분야의 선두주자인 지멘스는 심층적인 분야 전문성을 바탕으로 생성형 AI를 포함한 AI 기술을 실제 응용 분야에 적용해 다양한 산업의 고객이 AI를 접근 가능하고 효과적으로 활용할 수 있도록 한다. 또한 지멘스는 헬스케어 분야의 혁신을 선도하는 세계적 의료기술 기업이자 상장 계열사인 지멘스 헬시니어스의 최대 지분을 보유하고 있다. 지멘스는 모두를 위한 모든 곳에서의 지속 가능한 솔루션을 제공한다.

2025년 9월 30일 종료된 2025 회계연도에 지멘스 그룹의 매출액은 789억 유로, 순이익은 104억 유로다. 2025년 9월 30일 기준 전 세계적으로 31만 8천 명의 직원이 근무하고 있다. 자세한 내용은 https://www.siemens.com/에서 확인할 수 있다.

지멘스 관련 상표 목록은 여기에서 찾아볼 수 있다. 기타 상표는 해당 소유자에게 속한다.

언론 연락처