보도 자료

Siemens’ new PAVE360 Automotive drives next-generation vehicle development with real-world validation

2025년 12월 18일
Plano, Texas, USA

PAVE360 Automotive is a new category of digital twin software designed to address the escalating complexity of automotive hardware and software integration
  • New off-the-shelf, cloud-based, digital twin offering, PAVE360 Automotive, empowers automakers and suppliers to begin full-system development on day one, reducing setup time from months to days   
  • Delivers a fully integrated, system-level digital twin that speeds up development of advanced driver-assistance systems (ADAS), autonomous driving (AD) and in-vehicle infotainment (IVI) systems using the latest automotive technology from industry leaders like Arm
  • New PAVE360 Automotive digital twin blueprint to be demonstrated live for the first time at CES 2026

Today, Siemens, a leading industrial technology company, unveiled its PAVE360™ Automotive technology, a new category of digital twin software that is pre-integrated and designed as an off-the-shelf offering to address the escalating complexity of automotive hardware and software integration.

PAVE360 Automotive empowers automotive manufacturers and suppliers to speed the development of software-defined vehicles (SDVs) with early full-system, virtual integration that mirrors real vehicle hardware and accelerates both application and low-level software development for ADAS, AD and IVI. This removes the need for customers to build their own digital twins before testing software and significantly reducing time to market for critical applications – from months to days.

With vehicle hardware and software complexity rising at an unprecedented rate, development teams face mounting pressure to deliver innovation faster and compete with new market entrants while meeting increasingly sophisticated consumer expectations. Traditional development methodologies are no longer sufficient to manage system-level interdependencies between ADAS, AD and IVI functions - a new approach is required.

“The automotive industry is at the forefront of the software-defined everything revolution and Siemens is delivering the digital twin technologies needed to move beyond incremental innovation and embrace a holistic, software-defined approach to product development,” said Tony Hemmelgarn, president and CEO, Siemens Digital Industries Software. “PAVE360 Automotive will empower automotive companies to innovate with confidence, agility and scale, to realize the full potential of the SDVs and set the standard for what’s possible across all industries.”  

A person is standing in front of a Siemens Pavé 360 machine, which is used for testing and developing autonomous vehicles.

PAVE360 Automotive is a new category of digital twin software designed to address the escalating complexity of automotive hardware and software integration

PAVE360 Automotive: A virtual blueprint for digital twin development PAVE360 Automotive leverages Siemens’ expertise in digital twin technology empowers automakers to:  

  • Jumpstart vehicle systems development from the earliest phases with ADAS, AD and IVI customizable virtual reference designs 
  • Unify development, optimize efficiency and increase cloud-based collaboration with a single digital twin for all teams 
  • Customize and scale by adding software, models and external hardware as needed 
  • Speed up software development leveraging hardware-like simulation speed of the latest automotive IP, including the new Arm® Zena Compute Subsystem (CSS) 
  • Validate with real-world feedback by connecting digital twins to physical hardware and testing in real vehicles 

 System-level digital twins for SDVs using existing technologies can be complex and time consuming to create and validate. To solve this bottleneck, PAVE360 Automotive delivers a fully integrated, system-level digital twin that can be deployed on day one – reducing the time, effort and cost required to build such environments from scratch. 

PAVE360 Automotive using Arm

Following prior collaboration with Arm which resulted in accelerated virtual environments for its Arm Cortex-A720AE in 2024 and Arm Zena Compute Subsystems (CSS) in 2025, Siemens is now further integrating Arm Zena CSS with PAVE360 Automotive to enable the industry to start building on Arm faster and more seamlessly than ever before. Access to Arm Zena CSS in a digital twin environment like PAVE360 Automotive accelerates the development of software by up to two years.

“As vehicles become increasingly AI-defined, automakers and silicon partners need new ways to manage rising complexity without slowing innovation,” said Suraj Gajendra, vice president of products and solutions, Physical AI Business Unit, Arm. “With Arm Zena CSS available inside Siemens’ pre-integrated PAVE360 Automotive environment, partners can not only customize their solutions leveraging the unique flexibility of the Arm architecture but also validate and iterate much earlier in the development cycle, helping them get to market sooner.”

Availability

PAVE360 leverages Siemens’ Innexis™ software environment combined with supporting technologies to empower users to create system-level digital twins of ADAS, AD and IVI capabilities. Siemens’ PAVE360 Automotive is available to key customers, with general availability in February 2026 and will be demonstrated live at CES 2026 in the Auto Hall, January 6–9, 2026. Attendees are invited to experience how Siemens is helping pioneers to deliver the future of automotive innovation. To learn more about Siemens’ PAVE360 Automotive, visit https://blogs.sw.siemens.com/pave360/2025/12/18/pave360-automotive-what-is-an-sdv-digital-twin-blueprint-and-why-do-you-need-one/

Note for editors attending CES 2026: Roland Busch, President and CEO of Siemens AG, will deliver a keynote at CES 2026 to showcase how Siemens is developing AI, digital twin and automation technology to drive real-world impact and usher in a new era of AI-ready manufacturing, infrastructure and transportation. To register, visit CES 2026 registration.

지멘스 디지털 인더스트리 소프트웨어 소개

지멘스 디지털 인더스트리 소프트웨어는 규모에 상관없이 모든 기업들이 Siemens Xcelerator 비즈니스 플랫폼의 소프트웨어, 하드웨어, 서비스를 사용해 디지털 전환을 추진하도록 지원한다. 지멘스의 소프트웨어와 포괄적인 디지털 트윈을 통해 기업은 설계, 엔지니어링, 제조 프로세스를 최적화함으로써 오늘의 아이디어를 미래의 지속가능한 제품으로 만들어낼 수 있다. 칩부터 전체 시스템까지, 제품부터 프로세스까지, 모든 산업을 아우른다.Siemens Digital Industries Software – Accelerating transformation.

지멘스 디지털 인더스트리 소개

지멘스 디지털 인더스트리(DI)는 공정과 개별 제조 산업에 속한 모든 규모의 기업이 전체 가치사슬에서 디지털·지속가능성 전환을 가속화할 수 있도록 지원한다. 지멘스의 최첨단 자동화와 소프트웨어 포트폴리오는 제품과 생산의 설계, 구현, 최적화를 혁신적으로 개선한다. 개방형 디지털 비즈니스 플랫폼인 Siemens Xcelerator를 통해 보다 쉽고 빠르며 확장 가능한 프로세스를 구현할 수 있다. DI는 파트너·생태계와 함께 고객이 지속 가능한 디지털 기업이 될 수 있도록 지원한다. 전 세계적으로 약 7만여명의 직원들이 DI에 근무하고 있다.

지멘스 소개

독일 베를린과 뮌헨에 본사를 둔 지멘스는 산업, 인프라, 모빌리티, 헬스케어 등의 분야에 역량을 집중하고 있는 세계적인 기술 기업이다. 지멘스는 모든 사람을 위해 일상을 변화시키는 기술을 개발하는 것을 목적으로 한다. 지멘스는 현실과 디지털 세계를 결합함으로써 고객이 디지털과 지속 가능성 전환을 가속화해 보다 효율적인 공장, 살기 좋은 도시, 지속 가능한 운송을 구현할 수 있도록 지원한다. 산업용 AI 분야의 선두주자인 지멘스는 심층적인 분야 전문성을 바탕으로 생성형 AI를 포함한 AI 기술을 실제 응용 분야에 적용해 다양한 산업의 고객이 AI를 접근 가능하고 효과적으로 활용할 수 있도록 한다. 또한 지멘스는 헬스케어 분야의 혁신을 선도하는 세계적 의료기술 기업이자 상장 계열사인 지멘스 헬시니어스의 최대 지분을 보유하고 있다. 지멘스는 모두를 위한 모든 곳에서의 지속 가능한 솔루션을 제공한다.

2025년 9월 30일 종료된 2025 회계연도에 지멘스 그룹의 매출액은 789억 유로, 순이익은 104억 유로다. 2025년 9월 30일 기준 전 세계적으로 31만 8천 명의 직원이 근무하고 있다. 자세한 내용은 https://www.siemens.com/에서 확인할 수 있다.

언론 연락처