보도 자료

Siemens & PhysicsX collaborate to build AI-based deep physics simulation

2024년 12월 4일
Plano, Texas, USA

PhysicsX is building its latest pre-trained Large Physics Model (LPM) for aerodynamics on high-fidelity simulation data generated with Siemens’ Simcenter simulation software (image credit: PhysicsX)
  • AI startup’s release of its latest pre-trained deep physics model is built on high-fidelity data generated with Siemens’ Simcenter simulation software

Siemens Digital Industries Software announced today its ongoing collaboration with PhysicsX, a startup leveraging generative AI to enable breakthrough engineering in advanced industries. Together, they aim to create the next generation of AI-based deep physics simulation to accelerate performance prediction and optimization. PhysicsX is building its latest pre-trained deep physics model for aerodynamics on high-fidelity simulation data generated with the Siemens Xcelerator portfolio.

“AI represents a truly transformative opportunity for the simulation community, and we are exploring its potential at an accelerated rate,” said Jean-Claude Ercolanelli, senior vice president, Simulation and Test Solutions, Siemens Digital Industries Software. “To scale AI adoption, open collaboration is key and Siemens is delighted to see PhysicsX unveil to the world what it is working on – together, we’re exploring an AI-enhanced simulation industry that has the potential to change how products are ideated and engineered.”

“We are delighted to take our collaboration with Siemens to the next level, working together on fundamental technology to improve the way engineering is practiced,” said Robin Tuluie, founder and chairman of PhysicsX. “The basis for successful AI deployment into engineering hinges on highest-quality synthetic data, robust integrations between Computer Aided Engineering (CAE) and AI [Artificial Intelligence] and building on the trust customers have in our respective technologies. We are thrilled to be building into the opportunity space together with Siemens with the release of our latest Large Geometry Model (LGM) for aerodynamics, LGM-Aero, trained on high-fidelity data generated with Siemens Xcelerator portfolio tools. We are also delighted to be releasing Ai.rplane, an open-access reference application showcasing the power of LGM-Aero to design innovative aero solutions.”

Large Geometry Model (LGM) release Much of the promise of AI in industrial applications starts with the dramatic acceleration that AI can bring to simulation. PhysicsX’s LGM-Aero is trained on a corpus of more than 25 million geometries and associated physics simulation. The training data contains tens of billions of mesh elements and tens of thousands of Computational Fluid Dynamics (CFD) and Finite Element Analysis (FEA) simulations using high-quality Simcenter™ STAR-CCM+™ software and Simcenter™ Nastran software. It allows users to fine-tune deep learning models for their own applications with as little as a few tens of simulations.

Technology demonstrator goes live

A Siemens PhysicsX newsroom image featuring a person in a lab coat working on a computer.

PhysicsX has released Ai.rplane, a free-to-use public-access technology demonstrator offering a set of exploratory tools focused on aerodynamics and aircraft structures with unique AI-shape generation – built on training data created using Siemens’ Simcenter Nastran and STAR-CCM+ software. (Image credit: PhysicsX)

PhysicsX has also released Ai.rplane, a free-to-use public-access technology demonstrator offering a set of exploratory tools focused on aerodynamics and aircraft structures with unique AI-shape generation. Ai.rplane is the world’s first Large Physics Model (LPM) for flight, a fully trained model that generalizes to a broad set of aeroelastic applications. Ai.rplane can infer aero performance, flight stability and structural stress for any flying shape and is a true zero-shot model. This technology creates geometry and delivers results in less than a second, compared to the several hours required for traditional numerical simulations.

Siemens PhysicsX Newsroom image featuring a person in a lab coat with a scientific instrument in the background.

PhysicsX’s Ai.rplane is the world’s first Large Physics Model (LPM) for flight, a fully trained model that generalizes to a broad set of aeroelastic applications. (Image credit: PhysicsX)

Starting with a basic set of instructions, users can explore the full generative design space offered by Ai.rplane, then modify or optimize for a desired performance characteristic in seconds. Over time, PhysicsX aims to add new features, including cargo packaging, selection of commercial powertrains, and controls.

Ai.rplane was developed using an extensive set of simulation technologies from Siemens to automate the generation of high-quality training data. Both LGM-Aero and Ai.rplane are available on the PhysicsX AI engineering platform.

To access Ai.rplane go to airplane.physicsx.ai.

지멘스 디지털 인더스트리 소프트웨어 소개

지멘스 디지털 인더스트리 소프트웨어는 규모에 상관없이 모든 기업들이 Siemens Xcelerator 비즈니스 플랫폼의 소프트웨어, 하드웨어, 서비스를 사용해 디지털 전환을 추진하도록 지원한다. 지멘스의 소프트웨어와 포괄적인 디지털 트윈을 통해 기업은 설계, 엔지니어링, 제조 프로세스를 최적화함으로써 오늘의 아이디어를 미래의 지속가능한 제품으로 만들어낼 수 있다. 칩부터 전체 시스템까지, 제품부터 프로세스까지, 모든 산업을 아우른다.Siemens Digital Industries Software – Accelerating transformation.

지멘스 관련 상표 목록은 여기에서 찾아볼 수 있다. 기타 상표는 해당 소유자에게 속한다.

언론 연락처