Persbericht

A new type of protection solution for power grids

11 februari 2026
Hungary

Up to 60 hardware-based protection devices can be replaced with virtualization.

Virtualization, which has already proven itself in IT, is also playing an increasingly important role in electrical power networks. A new solution that has just been introduced can accelerate the expansion of power networks and reduce the space requirements of substation buildings.

The new Siprotec V combines the functionality of up to 60 hardware-based Siemens Siprotec 5 devices in a single server-based solution. These widely used intelligent protection and field control devices continuously monitor the electrical network and, in the event of a fault (such as a short circuit), disconnect the affected section, thus ensuring the continued reliable operation of the network.

A central AI system shows up to 25% lower investment costs, 45% less station-building space, and 50% lower CO₂ emissions.

Thanks to virtualization, Siprotec V enables comprehensive digital testing of substation protection and control technology as well as communication configurations even before commissioning. This not only simplifies installation, speeds up testing and minimizes errors, but also allows for quick adaptation to changing system requirements, regardless of hardware limitations. This facilitates the smooth introduction of software updates, fixes, and functional enhancements, as well as compliance with current and future cybersecurity standards.

Furthermore, replacing hardware devices means fewer switch cabinets, copper cables, and other physical equipment are required. This saves 25 percent of capital expenditure (CAPEX) costs per substation and half of the carbon dioxide emissions associated with installation and material use, while energy suppliers can save up to 20 percent of total life cycle costs.

Siprotec V also enables advanced artificial intelligence applications to run directly in the substation environment, providing power companies with real-time insight, predictive analytics, and better decision support.

Siemens AG (Berlin and Munich) is a leading technology company focused on industry, infrastructure, mobility, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably. In fiscal 2025, which ended on September 30, 2025, the Siemens Group generated revenue of €78.9 billion and net income of €10.4 billion. As of September 30, 2025, the company employed around 318,000 people worldwide on the basis of continuing operations. Further information is available on the Internet at www.siemens.com.

Contactpersonen voor de pers

Tel.: +36 (1) 471-1446
Email: kommunikacio.hu@siemens.com