Persbericht

Siemens accelerates engineering simulation with a unified AI-powered Simcenter portfolio

28 juli 2026
Plano, Texas, USA

  • New Simcenter portfolio combines Siemens and Altair simulation technologies to enable more comprehensive and connected engineering workflows
  • Expanded AI-driven simulation and GPU acceleration help engineers explore more designs and make decisions faster
  • New multiphysics workflows enable earlier insight, improved productivity and reduced development risk

Siemens today announced availability of the latest Simcenter software release with significant enhancements across the portfolio, delivering new capabilities that help engineers accelerate simulation workflows, explore more options faster and make more confident decisions earlier in the design process.

As engineering challenges grow in complexity, organizations are under increasing pressure to evaluate more design options while managing increasingly complex systems. The latest Simcenter updates address this need by enabling faster simulation, earlier insight and more connected workflows across disciplines.

This release is also the first to bring together Siemens and Altair simulation technologies in a unified simulation portfolio. By aligning these technologies within consistent workflows, Siemens helps engineering teams apply simulation more broadly, reduce complexity and improve decision-making.

“The future of engineering depends on an organization’s ability to turn insight into action faster than ever before,” said Sam Mahalingam, executive vice president, Simulation, Siemens Digital Industries Software. “We have brought together industry-leading simulation capabilities across physics domains, connected them in shared workflows and made simulation more accessible. This unified portfolio helps customers explore more possibilities sooner, scale simulation across teams and accelerate innovation with greater confidence.”

The AI-based capabilities within Simcenter portfolio help engineers reduce reliance on time-intensive simulation runs by identifying the most promising concepts earlier and delivering results in a fraction of the time associated with traditional workflows. This allows teams to iterate more quickly while focusing detailed simulation where it delivers the most value.

siemens-simcenter-summer-2026-02

Simcenter PhysicsAI can generate new physics-aware design concepts based on target dimensions, performance KPIs and historical training data in seconds - removing barriers to broad design space exploration

AI-accelerated innovation with Simcenter PhysicsAI: Simcenter PhysicsAI is now integrated across more products within the Simcenter portfolio. Simcenter PhysicsAI is Siemens’ geometric deep learning technology that transforms simulation data into high-fidelity predictive models that help engineers evaluate more concepts and make confident design decisions up to 1,000x faster than traditional solver simulations. Data and models generated with Simcenter PhysicsAI can be leveraged by Siemens’ Intelligence Center X, the new industrial AI orchestration software.

When integrated into Siemens’ Simcenter™ Inspire™ software, it enables engineers to predict results across a broad spectrum of analysis and production processes, from general purpose structural analysis through casting, molding, die stamping and extrusion processes. Additionally, Siemens’ PhysicsAI technology inside Simcenter Hypermesh has been extended for more efficient data training and greater confidence in results.

With the addition of multi-GPU support in Simcenter™ STAR-CCM+™ software, Simcenter PhysicsAI also allows engineers to train AI models from computational fluid dynamics (CFD) simulations significantly faster (achieving 10x speed improvements and beyond) and iterate with greater confidence.

Newly introduced is Simcenter PhysicsAI Generate, which allows teams to create novel and innovative design concepts in seconds using existing knowledge and product data. By using a physics-aware generative AI engine, it can generate new concepts based on target dimensions, performance KPIs and historical training data in seconds – radically removing barriers to broad design space exploration based on real physics.

siemens-simcenter-summer-2026-03

Integration of Simcenter Simsolid with Designcenter for advanced product engineering allows simulation to be run directly on the geometry without the need to create a mesh, allowing designers to quickly assess performance in minutes, not hours

Bringing simulation earlier in the design process: The updates also make simulation more accessible across the product lifecycle. Engineers can evaluate performance directly on 3D CAD models with minimal preparation, helping shift simulation earlier in the design process and accelerate decision-making. This is enabled through the integration of Simcenter™ Simsolid™ software with Siemens’ Designcenter™ software for advanced product engineering. Designcenter geometry is transferred seamlessly to Simcenter Simsolid, loads and constraints are added and run simulation directly on the geometry without the need to create a mesh, allowing designers to quickly assess performance in minutes, not hours.

siemens-simcenter-summer-2026-04

Simcenter PhysicsAI is Siemens’ geometric deep learning technology that transforms simulation data into high-fidelity predictive models that help engineers evaluate more concepts and make confident design decisions up to 1,000x faster than traditional solver

Delivering comprehensive multiphysics: The latest updates continue to deliver on Siemens’ mission to create the most comprehensive multiphysics simulation portfolio. A key focus is to enhance connections between multi-domain simulation technologies across complex systems, enabling more holistic design exploration.

For example, engineers can link electromagnetic, thermal and system simulation workflows more seamlessly, enabling earlier insight into performance of electric powertrain systems. New capabilities such as exporting reduced motor models from Simcenter™ Flux™ software into system and 3D simulation tools, alongside enhanced multiphysics simulation in Simcenter STAR-CCM+, help improve accuracy in areas such as motor cooling and battery thermal behavior while supporting more efficient collaboration across multi-disciplinary engineering teams.

Together, these advances support a more connected and AI enhanced approach to simulation as part of the Siemens Xcelerator portfolio, enabling a continuous flow of insight across design, validation and operation. The result is a practical and flexible simulation environment that helps organizations increase engineering speed, reduce development risk and deliver higher-performing products.

To learn more about the unified Simcenter portfolio and the broad range of enhancements and advances in the latest update, visit https://www.siemens.com/en-us/products/simcenter/latest-version/

Siemens Digital Industries Software helpt organisaties van elke omvang bij hun digitale transformatie met behulp van software, hardware en diensten van het Siemens Xcelerator-bedrijfsplatform. Dankzij de software van Siemens zoals zijn comprehensive digital twin kunnen bedrijven hun ontwerp-, engineering- en productieprocessen optimaliseren om ideeën om te zetten in de duurzame producten van de toekomst. Van chips tot complete systemen, van product tot proces, in alle sectoren. Siemens Digital Industries Software – Accelerating transformation

Opmerking: Een lijst met relevante handelsmerken van Siemens vindt u hier. Andere handelsmerken zijn eigendom van hun respectieve eigenaren.

Note: A list of relevant Siemens trademarks can be found here. Other trademarks belong to their respective owners.

Contactpersonen voor de pers

Siemens Digital Industries Software PR Team

Email: press.software.sisw@siemens.com