Informacja prasowa

Siemens introduces WATTBLOC utility-scale solar platform with model 500 string inverter and Virtual Central Station

16 listopada 2026
Las Vegas, NV

  • Assembled-in-the-USA platform combines the WATTBLOC 500 string inverter with a highly agile, modular and scalable Virtual Central Station architecture
  • Modular building blocks support cost-effective expansion, inherent redundancy, simplified serviceability and long-term fleet standardization

Siemens recently unveiled WATTBLOC™, its American-assembled utility-scale solar platform that brings together the WATTBLOC™ 500 string inverter and WATTBLOC™ Virtual Central Station architecture. Designed specifically for large-scale photovoltaic projects, the platform introduces a highly agile, modular and scalable approach to power conversion, giving utilities, developers, EPCs and asset owners greater flexibility in how solar plants are designed, deployed, expanded and maintained.

At the center of the platform is the WATTBLOC 500, a single-maximum power point tracking string inverter designed for utility-scale solar applications. The inverter supports multiple AC voltage configurations from 370 V to 800 V, with power ratings ranging from 227 kVA to 500 kVA depending on voltage selection. Its design incorporates silicon carbide technology, active cooling and a single-stage topology, achieving maximum efficiency of up to 99.2 percent while supporting stand-alone deployment or integration into a WATTBLOC Virtual Central Station.

NEMA 4X and IEEE 2800 compliant, the WATTBLOC 500 also serves as the building block for WATTBLOC Virtual Central Station, Siemens’ modular approach to utility-scale solar power conversion. The architecture combines multiple string inverter modules with AC switchgear and medium-voltage transformation to create repeatable power blocks that can scale from smaller project configurations of 1 MW to 5 MWac blocks, depending on the selected configuration.

Unlike traditional central inverter architectures that concentrate power conversion into a single large inverter, WATTBLOC Virtual Central Station distributes power conversion across multiple independent inverter modules. This distributed approach combines redundancy with serviceability. Individual modules can be isolated and serviced while remaining capacity continues operating, helping reduce downtime exposure and supporting higher overall plant availability. And because power conversion and controls are distributed across independent modules, the architecture is inherently resilient.

“Utility-scale solar should not require customers to choose between flexibility, scalability and reliability,” said Dave Pisano, Head of Utility Systems and Solutions for Electrification and Automation at Siemens Smart Infrastructure USA. “We designed WATTBLOC around a fundamentally different idea: make the power-conversion building block smaller, independent and incredibly flexible, and then allow customers to deploy it in the configuration that makes the most sense for their site. That combination of agility, modularity and redundancy gives customers a powerful platform for improving availability, simplifying maintenance and scaling their solar assets over time.”

WATTBLOC also reflects Siemens’ broader utility infrastructure experience by pairing power conversion technology with the electrical components needed for utility-scale deployment. By integrating inverter module technology with switchgear and medium-voltage transformation in a standardized architecture, Siemens is helping customers move beyond individual inverter selection toward an integrated, repeatable and scalable approach to solar power blocks designed for long-term ownership.

Available in 2027, the WATTBLOC 500 string inverter and WATTBLOC Virtual Central Station architecture will be on display at Siemens’ RE+ booth N3150 from November 16 – 19, 2026.

WATTBLOC is a trademark of Siemens and/or its affiliates in some countries.

About Siemens

Siemens Corporation is a U.S. subsidiary of Siemens AG, a leading technology company focused on industry, infrastructure, transport, and healthcare. The company’s purpose is to create technology to transform the everyday, for everyone. By combining the real and the digital worlds, Siemens empowers customers to accelerate their digital and sustainability transformations, making factories more efficient, cities more livable, and transportation more sustainable. A leader in industrial AI, Siemens leverages its deep domain know-how to apply AI – including generative AI – to real-world applications, making AI accessible and impactful for customers across diverse industries. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a leading global medical technology provider pioneering breakthroughs in healthcare. For everyone. Everywhere. Sustainably.

In fiscal year 2025, which ended on September 30, 2025, the Siemens Group USA generated revenue of $24.427 billion with 27 manufacturing sites across the U.S. and more than 50,000 employees serving customers in all 50 states and Puerto Rico.

Siemens Smart Infrastructure (SI) kształtuje rynek inteligentnej infrastruktury zarówno dziś, jak i przyszłości. Odpowiada na wyzwania związane z urbanizacją i zmianami klimatu, łącząc systemy energetyczne, budynki i przemysł. SI oferuje klientom kompleksowe portfolio od jednego źródła – produkty, systemy, rozwiązania i usługi od momentu produkcji energii aż po zużycie. Dzięki coraz bardziej cyfrowemu ekosystemowi pomaga klientom rozwijać się i rozwijać społeczności, jednocześnie przyczyniając się do ochrony planety. Promujemy kompleksowe cyberbezpieczeństwo, zapewniające bezpieczne i niezawodne operacje. Siemens Smart Infrastructure ma swoją globalną siedzibę w Zug, Szwajcaria. Na dzień 30 września 2025 roku firma zatrudniała około 79 400 pracowników na całym świecie.

Kontakt dla prasy

Allison Britt
Phone: +1-630-399-2587
Email: allison.britt@siemens.com