Comunicado de imprensa

Siemens accelerates physical testing with Simcenter Testlab

28 de setembro de 2026
Plano, Texas, USA

The latest updates to Simcenter Testlab software, helping engineering testing teams streamline complex testing processes
  • Next-generation Simcenter Testlab Neo workflows deliver up to 35 percent efficiency gains in structural dynamics testing and 60 percent faster noise, vibration and harshness (NVH) prediction
  • Creates AI-ready engineering data with improved annotation, validation and automation
  • Reduces risk in spacecraft and aerospace qualification tests through virtual shaker testing

Siemens today announced the latest updates to Simcenter™ Testlab™ software, helping engineering teams reduce manual work, deliver consistent results and make engineering decisions earlier. The new updates combine integrated testing workflows, automation and improved data management to accelerate the path from test setup to engineering insight. Enhancements span structural dynamics, system NVH prediction, AI-ready data preparation, and shock and vibration test preparation. These capabilities allow organizations to capture contextualized data earlier in development, supporting faster cycles and more informed decision-making.

"As products become more complex, engineering teams need to turn testing data into trusted insights," said Bruno Massa, vice president, Simcenter Testing Solutions, Siemens Digital Industries Software. "The latest Simcenter Testlab updates help teams deliver results faster, validate earlier, and build the foundation for AI-driven testing."

Key enhancements:

Accelerated engineering insights – The latest updates complete the transition toward next-generation workflows in Simcenter Testlab Neo software. Test engineers can execute integrated, end-to-end structural dynamics workflows with less manual effort, enabling non-experts to set up and execute tests consistently. These updates deliver up to 35 percent efficiency gains across the structural dynamics process. Additionally, new system NVH prediction workflows integrate component characterization with virtual prototyping, evaluating performance up to 60 percent faster before physical prototypes are built.

Simcenter Testlab Neo brings shaker acquisition, real-time visual setup feedback, and full Simcenter SCADAS hardware support

Simcenter Testlab Neo brings shaker acquisition, real-time visual setup feedback, and full Simcenter SCADAS hardware support into one unified structural dynamics testing environment helping users of any expertise level improve data quality and reduce setup errors

Building AI-ready data – Trustworthy AI requires structured, traceable and contextualized data. The latest updates integrate data acquisition, analysis and management into a single environment. Improved annotation and automation help teams create AI-ready datasets that are easily reusable. Simcenter Testlab also now complements physical test data with virtual data to train robust AI models.

De-risking critical testing earlier – New virtual shaker testing capabilities allow aerospace and defense teams to prepare for qualification and durability testing using simulation. By deriving models of the complete test setup, engineers can evaluate scenarios before applying full test levels to expensive physical hardware, reducing uncertainty and risk.

Simcenter Testlab 2606 introduces virtual shaker testing which helps engineers model the complete test setup, evaluate quali

Simcenter Testlab introduces virtual shaker testing which helps engineers model the complete test setup, evaluate qualification scenarios, and refine controller settings before testing valuable hardware—reducing uncertainty and risk during critical spacecraft test campaigns

Automated NVH engineering – A new automated component model extraction solution reduces manual work in creating reusable models for system-level NVH analysis. These ISO-compliant workflows help teams scale component characterization across projects, enabling earlier decision-making based on test-based inputs.

The new automated component model extraction solution industrializes the NVH component characterization process per ISO 2027

The new automated component model extraction solution industrializes the NVH component characterization process per ISO 20270. It automates the measurement and extraction workflow, enabling repeatable, high-throughput component testing with minimal manual intervention.

Unlocking more value from Simcenter SCADAS at no extra cost – Available license-free, Simcenter Testlab Go and Simcenter SCADAS Go simplify time data acquisition, monitoring and validation with Simcenter SCADAS hardware - eliminating license administration, dongles and network dependencies while expanding access, deployment flexibility and the value of existing hardware investments.

To learn more about the latest Simcenter Testlab updates, visit the Simcenter Testlab blog https://blogs.sw.siemens.com/simcenter/whats-new-in-simcenter-testlab-2606/

A Siemens Digital Industries Software ajuda empresas de todos os portes em sua transformação digital usando software, hardware e serviços da plataforma Siemens Xcelerator. O software da Siemens e o gêmeo digital abrangente permitem que as empresas otimizem seus processos de projeto, engenharia e manufatura para transformar as ideias de hoje em produtos sustentáveis do futuro. De chips a sistemas inteiros, de produtos a processos, para todos os setores. Siemens Digital Industries Software– Accelerating transformation.

Obs.: A lista de marcas comerciais relevantes da Siemens pode ser visualizada aqui. As outras marcas comerciais pertencem aos seus respectivos proprietários.

Contatos para imprensa

Siemens Digital Industries Software PR Team

Email: press.software.sisw@siemens.com