Comunicato stampa

Siemens extends Veloce hardware-assisted verification and validation with new Innexis shift-left software

7 novembre 2024
Plano, Texas, USA

  • Innexis delivers a set of products and capabilities to address demand for shift-left software development in the IC development process
  • With more demanding software workloads, it is critical to facilitate the development and execution of realistic workloads early in the design phase to shorten overall development time and identify hardware and software defects earlier

Siemens Digital Industries Software announced today the Innexis product suite, a complement to its industry leading Veloce™ hardware-assisted verification and validation system.

Building on the success and rapid adoption of Veloce, Siemens’ Innexis product suite delivers a set of capabilities to address customer demand for shift-left software in the early phases of IC development. These products include a hardware/software development flow from virtual to hybrid to full RTL, an architecture native virtual platform for early high-speed software development and a simulation backplane that enables the development of digital twins in Siemens’ PAVE360™ software for software-defined vehicles and other complex systems.

“The complexity of integrated circuits (IC) is increasing exponentially, designers need more efficient methodologies to meet industry demands. Veloce has seen rapid adoption by industry leaders to help solve this critical bottleneck. The Innexis product suite extends workflow improvements from Veloce to help our customers shift left their IC development and debug cycle,” said Jean-Marie Brunet, vice president and general manager, Hardware-Assisted Verification, Siemens Digital Industries Software. “This enables IC design to begin months before final RTL, all while using a common software workload across the development process.”

Adoption of a shift-left approach for software development and IP verification processes is now mandatory. As chip designs become increasingly complex due to more demanding software workloads, it is critical to enable the development and execution of realistic workloads early in the design phase. A proactive shift-left software approach helps mitigate the risk of identifying issues late in the development cycle.

“The implementation of Innexis in our development process has significantly enhanced software and system validation performance, thereby improving the efficiency of our teams and projects. By enabling heterogeneous component modeling within virtual platforms, it allows us to create realistic high-speed models of System on Chips (SoCs),” said Ari Hautala, Principal System Architect, Nokia Mobile Networks. “Furthermore, the integration of these high-speed virtual platforms with RTL IP on Veloce emulators facilitates superior overall performance while still permitting precise cycle-accurate performance and power analysis on RTL model components. Additionally, Innexis offers exceptional visibility and debuggability for the SoC design, along with the capability to integrate and execute a large number of complex test cases effectively.”

Currently, the Innexis product suite consists of:

Innexis Developer Pro: Innexis Developer Pro software provides a connected development flow from virtual to hybrid to full RTL. This provides a comprehensive environment for accelerating the creation of complex SoC design supporting a wide range of use-cases including seamless hardware-software co-development, co-validation, and pre-silicon cycle accurate analysis and validation. Innexis Developer Pro supports the modelling of complex SoC’s with heterogeneous cores and custom SystemC model components. In addition, it provides the ability to run in both virtual plus RTL hybrid mode for high performance execution, and then at a time of interest switch to full RTL emulation enabling high accuracy analysis of the full SoC when required.

Innexis Architecture Native Acceleration (ANA): Innexis Architecture Native Acceleration software is a cloud- based high-speed virtual platform. By running natively on Arm based servers the software workloads run at much higher speeds than on typical instruction set simulation based virtual platforms. Cloud hosting also provides scalable compute resources and simple browser-based access and tools. Innexis Architecture Native Acceleration can also run on local Arm based servers if preferred. In both cases it enables early software development and testing, and early software defect identification.

Innexis Virtual System Interconnect: Innexis Virtual System Interconnect software facilitates the creation and simulation of comprehensive system level digital twin platforms by seamlessly connecting multi-behavioral virtual and physical subsystems, supporting a variety of communication protocols. Innexis Virtual System Interconnect behavioral models can include Innexis Developer Pro or Innexis Architecture Native Acceleration SoC models, supporting system-level shift-left software development and RTL verification.

To learn more about Siemens’ Innexis product suite and how it addresses the demand for shift-left software development in the integrated circuit development process, visit: www.siemens.com/innexis

Siemens Digital Industries Software aiuta le organizzazioni di tutte le dimensioni ad affrontare la digital transformation utilizzando il software, l’hardware ed i servizi della piattaforma di business Siemens Xcelerator. Il software offerto da Siemens, unitamente alle tecnologie per la realizzazione di completi digital twin, consentono alle aziende di ottimizzare i propri processi di progettazione, di ingegnerizzazione e di produzione, per trasformare le idee di oggi in prodotti sostenibili del futuro. Da singoli chip fino a interi sistemi, dai prodotti ai processi, in tutti i settori. Siemens Digital Industries Software– Accelerating transformation.

Nota: un elenco dei marchi rilevanti di proprietà di Siemens è consultabile qui. Tutti gli altri marchi menzionati appartengono ai rispettivi proprietari.

Contatti per la stampa

Zulmira Almeida

Tel: (+33) 06 77 19 80 52; E-mail: marie.almeida@siemens.com

Anna Romanelli - ITALMARCO

Tel: (+39) 02 70 10 46 45 – (+39) 347 745 04 09; E-mail: anna@italmarco.com